What is BSP and PSP ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is BSP and PSP ?

8,119 次查看
Glogov_Kolac
Contributor II

Can someone explain me the meaning of theese terms. I am new in CORTEX M4 ?

4 回复数

4,551 次查看
mjbcswitzerland
Specialist V

Hi

 

See http://www.freescale.com/files/32bit/doc/app_note/AN4287.pdf for BSP (Board Support Packages)

 

PSP is not defined there but I am guessing that it may mean Project Support Package(?)

 

Regards

 

Mark

 

0 项奖励
回复

4,551 次查看
Nouchi
Senior Contributor II

Hi,

 

IMHO, PSP means Processor Support Package ?

 

Regards,

 

Emmanuel

4,551 次查看
Glogov_Kolac
Contributor II

It isunbelievable that there is no official explanation by Freescale of theese 2 terms !

0 项奖励
回复

4,551 次查看
Dekiru
Contributor IV

Hi Kolac,

 

Freescale mentions that in Glossary section of MQX User Guide (MQXOG.pdf)

 

BSP

Board support package. A group of files that are specific to a particular type of processor on a particular type of board. It includes drivers.

 

PSP

Processor Support Package. A group of file that are specific to a CPU type.

Regards