What code is running on a TWR-K70 out of the box?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What code is running on a TWR-K70 out of the box?

1,574 Views
720adams
Contributor I

Does anyone know what project code is running on a TWR-K70 right out of the box?

Labels (1)
0 Kudos
Reply
2 Replies

1,486 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Michael,

Please download the sample code of the TWR-K70 through the link as below.

https://cache.freescale.com/files/microcontrollers/software/app_software/code_examples/KINETIS_120MH...

Hope this helps!
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,486 Views
720adams
Contributor I

Thanks.  I will go through these, but I'm still not sure which sample code from which directory it is that is running on the TWR-K70.  It lights the leds when you tip the accelerometer on the board at different angles.  I'd like to know this before I erase the board's flash and can't put it back to the default state.

Mike

0 Kudos
Reply