What can erase/corrupt EEPROM data?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What can erase/corrupt EEPROM data?

1,396件の閲覧回数
Rigolon
Contributor II

Hello,

I have an application using MK22FX512AVLQ.

I've been using it for more than two years, but recently it started showing a weird behavior. So i checked it's memory.

The EEPROM sector where I save some parameters had some invalid values. Almost all, if not all of them had 0xFF.

I thought that maybe my device was getting powered off while erasing/writing into the EEPROM.

Unfortunately i can't share my code since it's from work, so here are some relevant info.

  • We save three different things in the EEPROM.

One sector (4KB) starting at 0x43000 with parameters

Four sectors starting at 0x44000 with user logs

Forty-nine sectors starting at 0x49000 with device logs

  • Only the sector with parameters gets erased/corrupted
  • I've looked at the code each time EEPROM gets re-written and every thing seems ok.
  • It happened three times between March and July of this year, but never happened before.
    The problem showed first, on each time, after being powered off and then on next day.
  • In one case all sector starting at 0x43000 got erased except for addresses from x043044 to 0x43047
  • In another case the addresses 0x43000 through 0x4304F, was left intact and the rest erased.

We are using some components that we bought 2021/2022 from a broker, when we couldn't find it anywhere else and it came in a pretty bad package (not sealed, no desiccant packs) only with an ESD plastic bag.

Since i have some data saved between beginning and ending of the sector on the first case, I'm not sure that the cause was powering of while erasing/writing new data to EEPROM.

Anyone has any idea of what could be doing this?

Thank you in advance

ラベル(1)
0 件の賞賛
返信
1 返信

1,338件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You said that "We are using some components that we bought 2021/2022 from a broker, when we couldn't find it anywhere else and it came in a pretty bad package (not sealed, no desiccant packs) only with an ESD plastic bag.", generally, we suggest you order the MCU from NXP distributor or NXP directly, otherwise, the chip quality can not be guaranteed.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信