What RTOS can I use with FRDM-KE06Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What RTOS can I use with FRDM-KE06Z?

ソリューションへジャンプ
3,130件の閲覧回数
jefersonip
Contributor III

Hello guys,

I wonder how to use an RTOS in FRDM-KE06Z in KDS go on a baremetal project.

Is that possible?

It seems that the MQX does not support this hardware.

Thanks,

ラベル(2)
0 件の賞賛
返信
1 解決策
2,656件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jeferson,

I'm using FreeRTOS with that board. Attached is a project which is available as well on SourceForge (mcuoneclipse/Examples/KDS/FRDM-KE06Z/FRDM-KE06Z at master · ErichStyger/mcuoneclipse · GitHub ).

This project is using Processor Expert (without Kinetis SDK). The project uses McuOnEclipse components available from SourceForge (see McuOnEclipse Releases on SourceForge | MCU on Eclipse ). You can use that FreeRTOS port without Processor Expert too (bare).

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,656件の閲覧回数
davidsherman
Senior Contributor I

MQX-Lite is supported on the KE06, though you use it through Processor Expert.  I haven't had experience with the other ones mentioned, but I have been using MQX-Lite on the KE06 for over a year now.

2,656件の閲覧回数
jefersonip
Contributor III

Very good, I have several options. I'm going to try the MQX-Lite so I want to try not to depend on a lot of Processor Expert. Thanks guys.

0 件の賞賛
返信
2,656件の閲覧回数
mjbcswitzerland
Specialist V

Hi

For a solution that will allow a project to run on most processors from KE02 up to K80 see

http://www.utasker.com/kinetis/FRDM-KE06Z.html

Regards

Mark

2,656件の閲覧回数
jefersonip
Contributor III

Thank you,

I am using the IDE KDS and must rtos who is supported in project of type baremetal, without using KSDK.

I tried portable BRTOS system, but without success.

I did not understand how portable FreeRTOS for this IDE.

If you have any idea, I would be very grateful.

0 件の賞賛
返信
2,657件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Jeferson,

I'm using FreeRTOS with that board. Attached is a project which is available as well on SourceForge (mcuoneclipse/Examples/KDS/FRDM-KE06Z/FRDM-KE06Z at master · ErichStyger/mcuoneclipse · GitHub ).

This project is using Processor Expert (without Kinetis SDK). The project uses McuOnEclipse components available from SourceForge (see McuOnEclipse Releases on SourceForge | MCU on Eclipse ). You can use that FreeRTOS port without Processor Expert too (bare).

I hope this helps,

Erich

0 件の賞賛
返信
2,656件の閲覧回数
jefersonip
Contributor III

Hello Erich,

Is very good,

Really works, now just adapt my codes.

Thanks,

0 件の賞賛
返信