We would like to develop a hardware and software project based on uP MK60FX512VLQ12....

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We would like to develop a hardware and software project based on uP MK60FX512VLQ12....

1,231 Views
paoloziveri
Contributor I

We would like to develop a hardware and software project based on uP MK60FX512VLQ12,
especially because it integrates EEPROM / FlexRam 16KB.

For this device the evaluation board  is TWR-K60F120M (see KINETISKMCUSELGD guide page 18 and page 24).


This card mounts MK60FN1M0VD12, in this uP is not present the 'EEPROM / FlexRam.
In the development system Kinetis Design Studio is not possible select TWR-K60F120M,
but we can create a project with the MK60FN1M0xxx12 device.

 

1) If we develop the project with Kinetis Design Studio with device MK60FN1M0xxx12
     we can transfer it and test it on the TWR-EVB K60F120M?

2) What do you suggest as an alternative to evaluate the MK60FX512VLQ12 before
   realize the hardware?
  
   Thanks.
   Regards

   

Paolo Ziveri

Labels (1)
0 Kudos
Reply
1 Reply

1,153 Views
jorge_a_vazquez
NXP Employee
NXP Employee

HI Paolo Ziveri

 

TWR-K60F120M uses MK60FN1M0VLQ12, and since you have a MK60FX512VLQ12, both of them have same features, with the differences of 'N/X' and '1M0/512' witch mean:

 

163810_163810.pngpastedImage_1.png

 

In KDS (Kinetis Design Studio) you should have to select MK60FX512xxx12, not MK60FN1M0xxx12

 

Hope this helps, please tell me if you have any more question on this.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply