We are facing a drift in RTC of the Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

We are facing a drift in RTC of the Processor

6,083件の閲覧回数
vikassingh
Contributor I

Hi Team,

In processor, "MK70FN1M0VMJ12" we are facing a clock drift in RTC during both Power on and Power off condition. During Power off, a coin battery(CR2032) is used as power source. Also this drift is not constant. It is varying. Operating temperature is within range of 20 deg Celsius to 35 deg Celsius. Maximum drift of 12 seconds per day is observed. I had attached RTC and crystal section of our schematic. Please help us further in resolving this issue. Is compensation register usage solves this issue? Please help as ASAP.

0 件の賞賛
返信
2 返答(返信)

5,749件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

From K70 reference manual, please refer below RTC crystal circuit design:

pastedImage_1.png

TWR-K70F120M board also using the same connection:

pastedImage_2.png

About RTC compensation, please refer application note AN4949 for the detailed info.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,749件の閲覧回数
vikassingh
Contributor I

For more details I am adding RTC Calculation also.

Crystal Part NumberABS07-32.768KHZ-7-T
Temperature Coefficient-0.036 ppm/˚C
S.No.Operating Temerature (˚C)Crystal Frequency Error (PPM)Error/Day (Seconds/day)
1-40-152.1-13.14144
2-30-108.9-9.40896
3-20-72.9-6.29856
4-10-44.1-3.81024
50-22.5-1.944
610-8.1-0.69984
720-0.9-0.07776
82500
930-0.9-0.07776
1040-8.1-0.69984
1150-22.5-1.944
1260-44.1-3.81024
1370-72.9-6.29856
1480-108.9-9.40896
1585-129.6-11.19744
0 件の賞賛
返信