Watchdog reset timeout value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Watchdog reset timeout value

3,017件の閲覧回数
Sourdev
Contributor II

I am using S9KEAZN64AMLC MCU (custom board). I configured Watchdog in window mode using an internal oscillator (32KHz). 

Configured watchdog timeout value is 500 msec.

when 256 clock Prescaler is enabled then the watchdog timer will reset at 534 msec and when 256 clock Prescaler is disabled then the watchdog timer will reset at 518 msec.

why it is taking more time to reset? 

when I use an External oscillator with 16Mhz, it resets at 508msec.  With an external oscillator, I am getting correct results but the internal oscillator and LPO creating problems (Not resetting at the exact timeout).

 

I checked with different timeout values and both oscillators, Please see the below table.

 

Internal Oscillator (32Khz)

 

External Oscillator (16Mhz)

Msec

Actual reset time (In msec)

Difference (In Msec)

 

Timeout value (in msec)

Actual reset time (In msec)

Difference (In Msec)

100

108

8

 

100

106

6

200

211

11

 

200

206

6

300

313

13

 

300

306

6

400

415

15

 

400

406

6

500

517

17

 

500

506

6

600

619

19

 

600

605

5

700

722

22

 

700

706

6

800

824

24

 

800

806

6

900

927

27

 

900

906

6

1000

1.028

0.028

 

1000

1.006

0.006

2000

2.05

0.05

 

 

 

 

How I can get the exact watchdog reset time with the internal oscillator?

NOTE: Observed the Same result with normal watchdog and Window watchdog. 

 

0 件の賞賛
返信
2 返答(返信)

3,000件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

The frequency of internal reference clock is factory trimmed to 31.25 kHz. Did you check the value of Watchdog Timeout Value Register? 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,940件の閲覧回数
Sourdev
Contributor II

Hi Robin Shen,

You are correct internal reference clock is factory trimmed to 31.25 kHz. Now I am getting the correct results.

Thank you for the support!!!!!!!!!

 

0 件の賞賛
返信