Watchdog LPO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Watchdog LPO

2,000 Views
martindusek
Contributor V

Hello,

I configured watchdog to run from LPO clock source on MK20DN512VLL10. However, I get watchdog reset everytime when the configured watchdog timeout passes, despite of refreshing the watchdog.

When I change the watchdog to run from BUS clock, it behaves as expected

Are there any precautions when running watchdog from LPO?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,476 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Martin

Thank you for the patience.

I do a test based on TWR-K60D100M board with mask set 2N22D.

I use below test code to set WDOG clock source is LPO and it works as expected.

Please check my test code below:

void test_wdog_lpo(void)

{

    wdog_unlock();

      /* WDOG_TOVALH: TOVALHIGH=0x0C00 */

  WDOG_TOVALH = 0x0; /* Setup time-out value register high */

  /* WDOG_TOVALL: TOVALLOW=2 */

  WDOG_TOVALL = 0x270F; /* Setup time-out value register low */

  /* WDOG_PRESC: ??=0,??=0,??=0,??=0,??=0,PRESCVAL=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  WDOG_PRESC = WDOG_PRESC_PRESCVAL(0x00); /* Setup status register */

  /* WDOG_STCTRLL: INTFLG=1,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=1 */

  WDOG_STCTRLL = (WDOG_STCTRLL_INTFLG_MASK | 0x01U); /* Setup status register */

  /* WDOG_STCTRLH: ??=0,DISTESTWDOG=1,BYTESEL=0,TESTSEL=0,TESTWDOG=0,??=0,??=1,WAITEN=1,STOPEN=1,DBGEN=0,ALLOWUPDATE=0,WINEN=0,IRQRSTEN=1,CLKSRC=1,WDOGEN=1 */

  WDOG_STCTRLH = 0x1F1;

}

void wdog_unlock(void)

{

  /* NOTE: DO NOT SINGLE STEP THROUGH THIS FUNCTION!!! */

  /* There are timing requirements for the execution of the unlock. If

   * you single step through the code you will cause the CPU to reset.

   */

  /* This sequence must execute within 20 clock cycles, so disable

         * interrupts will keep the code atomic and ensure the timing.

         */

        DisableInterrupts;

  /* Write 0xC520 to the unlock register */

  WDOG_UNLOCK = 0xC520;

  /* Followed by 0xD928 to complete the unlock */

  WDOG_UNLOCK = 0xD928;

  /* Re-enable interrupts now that we are done */

        EnableInterrupts;

}

I use below code to refresh the WDOG:

    /* Write 0xA602 to the refresh register */

  WDOG_REFRESH = 0xA602;

   /* Followed by 0xB480 to complete the refresh */

  WDOG_REFRESH = 0xB480;

Without refresh WDOG, it will generate chip reset every 10 seconds.

Wish it helps.

0 Kudos
Reply

1,476 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Martin,

I am checking with this issue, I will be back when I could get any updated info.

Thank you for the patience.

B.R.

Ma Hui

0 Kudos
Reply