**WARNING!** Bug Kinetis Bare Metal Same Code for SAI KINETIS_50MHZ_SC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

**WARNING!** Bug Kinetis Bare Metal Same Code for SAI KINETIS_50MHZ_SC

1,213 Views
eli_hughes
Contributor V

This applies to

Kinetis 50MHz bare metal sample code.  Size (K): 39831 Format: zip Rev #: 1.5 Modified: 4/2/2013

The function sai_mclk_config has a parameter "divide".    the variable is declared as a unsigned char but need to be at least a uint16_t.     The Divide portion of the I2S_MDR_REG is 12 bits in length so parameter needs to be able to store a bigger value.

0 Kudos
Reply
1 Reply

1,052 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Eli,

Thank you for the info.

Our Kinetis product team has known this issue, we are in processing to fix that issue in updated SAI driver.

Best regards,

Ma Hui

0 Kudos
Reply