Comparator Input Offset Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Comparator Input Offset Voltage

1,211 Views
admin
Specialist II

Hi,

I was looking at the comparator specifications for the KL04. The max input offset voltage is set to be 20mV. Where can I find the offset voltage range for the entire temperature operating range?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,125 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Goutam

This 20mV offset is the input analog voltage in full temperature range. The offset error will not

Hope my reply can help you.

Best Regards

Paul

0 Kudos
Reply