Voltage and Current MK64FN1M0VLQ12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage and Current MK64FN1M0VLQ12

1,573件の閲覧回数
gerardohernande
Contributor I

How much voltage can recive a mk64fn1m0vlq12 in its GPIO? Some people say 3.3V and others 5. I am a little confiuse, what is the best voltage to operate? And how much current a mk64fn1m0vlq12 can give in total (with all its pins high, using as outputs)?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,407件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The answer of Mark is right.

Also note that the port pins of MK64FN1M0VLQ12 are only 5V tolerant as inputs. The outputs are not 5V tolerant, and that includes pins configured as open-drain outputs. In output mode, if the pin is pulled above VDD, it will cause the output buffer to drive the output at VDD, which will pull-down the pin voltage to near VDD.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信