VREGIN on KL26

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VREGIN on KL26

1,185件の閲覧回数
paddythomas
Contributor I


I have just made a PCB incorporating the MKL26Z128, and am having difficulty getting it working as a USB device. I completely overlooked the VREGIN pin which powers the USB transceiver, so left this unconnected originally. I managed to solder the pin to the 3.3V supply on my PCB, and this allowed a host to detect the device, however, no actual data could be transferred. Looking on the scope shows the D+ pin at 3V and the D- pin at 0V - is this normal behaviour in idle (unconnected) state? Does the VREGIN pin require 5V to operate correctly? The datasheet seems to hint that 2.7-5.5V is acceptable.

I included a regulator on the PCB to provide the 3.3V supply. I have a current requirement of about 200mA, and I believe the onboard regulator on the MKL26Z128 is limited to 120mA. Is there any benefit to utilising the onboard VREG for power, or is it fine just to use the external regulator?

ラベル(3)
0 件の賞賛
返信
1 返信

1,088件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Paddy,

There is an internal 5V to 3.3V regulator for Kl26, the regulator output is VOUT33, which should be connected to a 4.7uF capacitor. So the VREGIN pin should be connected to 5V power supply instead of 3.3V power supply.

Hope it can help you.

BR

Xiangjun Rong

0 件の賞賛
返信