VREFH and VREFL connections for K60 when not using ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VREFH and VREFL connections for K60 when not using ADC

960 Views
tommyb
Contributor I

I am trying to determine if I can tie my VREFH and VREFL lines directly to digital ground if I am not using the ADC of the K60.  I of course would keep VDDA connected to VDD, and put a decoupling cap on VREF_OUT, but wondering if I need to decouple VREFH and VREFL if I am not using them.

0 Kudos
Reply
1 Reply

695 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tommy:

The recommendation is to connect VREFH to VDD and VREFL to GND. This helps with the noise immunity.


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply