VDD RELATION TO GPIO VOLTAGE LEVEL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VDD RELATION TO GPIO VOLTAGE LEVEL.

1,667件の閲覧回数
priyangeorge
Contributor I

Hi there,

      I am using mkl25z128vlk4 in one of my project. I want to drive the controller at 2.8V in my circuit to avoid level conversion required if i drive the same @3.3V. I want to know whether the gpio high voltage level is equal to vdd . i.e if I am applying 2.8V at Vdd pin will the gpio high level be 2.8V. I am kind of new with this controller and on a tight schedule. Any kind of help is appreciated.    

Regards,

Priyan George

ラベル(2)
0 件の賞賛
返信
1 返信

1,505件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi priyan george,

     About the higher level in the MCU, you can find it in the KL25 datasheet.

   http://www.nxp.com/files/32bit/doc/data_sheet/KL25P80M48SF0.pdf?fasp=1&WT_TYPE=Data%20Sheets&WT_VEND... 

    The input high voltage:

pastedImage_2.png

   The output high level:

pastedImage_3.png

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信