Using USB CDC causes a Watchdog Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB CDC causes a Watchdog Interrupt

1,456 Views
colemanmoore
Contributor I

I'm using the USB CDC with the k22f12810 part and after 10-15 writes of data using "USB_Class_CDC_Send_Data()" the program stops at the watchdog interrupt.  The watchdog is disabled at the beginning of the program.

Any suggestions?

Coleman

Labels (2)
0 Kudos
Reply
1 Reply

1,370 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Coleman Moore,

Which version of the USB stack you are using? Would you please provide more details of the demo run on your board? Thanks for your patience!


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply