Using USB CDC causes a Watchdog Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using USB CDC causes a Watchdog Interrupt

1,440件の閲覧回数
colemanmoore
Contributor I

I'm using the USB CDC with the k22f12810 part and after 10-15 writes of data using "USB_Class_CDC_Send_Data()" the program stops at the watchdog interrupt.  The watchdog is disabled at the beginning of the program.

Any suggestions?

Coleman

ラベル(2)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Coleman Moore,

Which version of the USB stack you are using? Would you please provide more details of the demo run on your board? Thanks for your patience!


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信