Using PDB and other timer, together at the same time on K53 family?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using PDB and other timer, together at the same time on K53 family?

2,798件の閲覧回数
lucacampanale
Contributor I

Hi,

I have the following problem:

My "software" on a Kinetis K53 family MK53DN512ZCLQ10 implements a DMA driven DAC for audio speaker, using PDB. And so far so good.

The problem occurs when for other stuff I decide to use, at the same time, another K53-timer e.g., FTM or PIT, together with PDB; in this case DMA driven DAC routine doesn't work.

Any idea? Is it possibile that PDB cannot work together with other timer such as FTM or PIT?

What's wrong?

Thank you all !!!

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

2,595件の閲覧回数
perlam_i_au
Senior Contributor I

Hi Luca:

Please check on the Errata e4588 on document attached, this could explain this behavior.


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信