Using Kinetis SPI without SIN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using Kinetis SPI without SIN

跳至解决方案
2,147 次查看
myke_predko
Senior Contributor III

I'm using a SPI port to write data to just an OLED display, there is no SPI data output that I would connect to the SPI SIN - currently I'm tying the pin to VSS.  

So, the obvious question is, could I use the pin I've allocated for SIN as a DI/DO and ignore what happens inside the chip?  Reading the RM, I don't see how this could be a problem, but I thought I'd ask the wise people here.  

标签 (1)
标记 (5)
1 解答
2,042 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

If the SIN do not influence the communication between the master and slave, you can ignore it. And use it as general IO. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,043 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

If the SIN do not influence the communication between the master and slave, you can ignore it. And use it as general IO. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,042 次查看
myke_predko
Senior Contributor III

Thank you - it's nice getting the extra pin.  

Have a great day!

0 项奖励
回复