Using FlexCAN on TWR-K60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using FlexCAN on TWR-K60N512

1,424件の閲覧回数
marcusviniciusm
Contributor I

Hello guys,

I'm testing my development kits: TWR-K60N512 and TWR-K60D100M

At first,  I tested the modules worked with the same program on both kits, but the FlexCAN  is not running at the TWR-K60N512

someone already had a similar problem?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,248件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

We don't find any issue with using K60 FlexCAN module.

For Kinetis K60 100MHz products with two silicon version, silicon 1.x (TWR-K60N512) with silicon 2.x (TWR-K60D100M).

Customer could download Kinetis 100MHz silicon 2.x example code (KINETIS512_V2_SC) from below link:

IAR KickStart™ Kinetis K60 Tower System|Freescale

I attached the Kinetis 100MHz silicon 1.x FlexCAN example code for you reference.

Customer also need to check the TWR-SER setting and connection.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------