Using FRDM-KL27Z Capacitive Touch Slider?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using FRDM-KL27Z Capacitive Touch Slider?

2,381件の閲覧回数
jjlange91
Contributor I

I recently picked up a FRDM-KL27Z board and I was hoping to use the capacitive touch slider as an interface for the project I am developing.  As far as I can tell, though, it looks like none of the KL27 series parts have the Touch Sensor Interface hardware, and I haven't seen any example code for using capacitive sense on this board.  Is there a supported method for capacitive sensing on this MCU?

Thanks.

ラベル(2)
0 件の賞賛
返信
1 返信

1,856件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Josh,

As you know the KL27 doesn't have the TSI module, however the TSS library offer the GPIO low level sensing method to measure the capacitance by using the GPIO capacitive touch sensing method, and please learn the more information through the links as below.

http://cache.nxp.com/files/sensors/doc/ref_manual/TSSAPIRM.pdf?fpsp=1&WT_TYPE=Reference%20Manuals&WT...

Touch-Sensing Software|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信