Using FRDM-KL05 board as external debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using FRDM-KL05 board as external debugger

ソリューションへジャンプ
2,552件の閲覧回数
pgo
Senior Contributor V

Hi All,

I've used the other FRDM boards as external debuggers using USBDM but I have found what I believe is an error on the FRDMKL05 board.

On the other FRDM boards there is a normally-closed jumper that isolates the SWCLK signal between the on-board chip and the 10-pin SWD connector while leaving the SWCLK connected between the K20 debugger chip and the 10-pin SWD connector.  This allows the connection of an external target for debugging.

The corresponding jumper on the FRDL-KL05 completely isolates the 10-pin connector and I cannot see an purpose for this.

Is there something I'm missing?

Is this likely to be changed in future revisions?

The jumper in question is J6 on the FRDM-KL05 schematic:

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL05Z_SCH.pdf?fpsp=1

bye

0 件の賞賛
返信
1 解決策
2,171件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi pgo,

yes, this is a known bug.

See Debug External Processors with USBDM and Freedom Board | MCU on Eclipse which has the hardware fix for it described.

I have reported this schematic error to Freescale, and the wanted to have it fixed in a next board revision. I have not seen such a new board revision yet. Until then, the above workaround needs to be applied.

I hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,171件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi pgo,

yes, this is a known bug.

See Debug External Processors with USBDM and Freedom Board | MCU on Eclipse which has the hardware fix for it described.

I have reported this schematic error to Freescale, and the wanted to have it fixed in a next board revision. I have not seen such a new board revision yet. Until then, the above workaround needs to be applied.

I hope this helps.

0 件の賞賛
返信
2,171件の閲覧回数
pgo
Senior Contributor V

Thanks Erich

bye

0 件の賞賛
返信