Using DMA with UART, with and without FIFO buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using DMA with UART, with and without FIFO buffer

ソリューションへジャンプ
2,777件の閲覧回数
panchogalactico
Contributor II

Hi. I´m having problems with the DMA. I use a k20 MCU, clocked to 72MHz.

I want to receive 8 bytes in the UART0, filling the RX buffer FIFO, and then move them to a int mem[8] array.

I can´t make it work. My question is about UART0_D register, because, as I understand, I have to read 8 successive times that register to get the 8 bytes, and the DMA machine increment the source pointer automatically after every read. So, How do I do it?. Can i force the DMA machine to keep the source pointer pointing to UART0_D while the destiny pointer incrementing automatically?

Actually, if I can force the DMA machine to do that, I guess that I didn't need to use the RX buffer FIFO.

Any ideas?

 

sorry for my poor english.

0 件の賞賛
返信
1 解決策
2,192件の閲覧回数
panchogalactico
Contributor II

I make it work, so I post here the answer.

If I set DMA_TCDn_SOFF = 0 , then the source pointer wont increment.

very easy actually.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,193件の閲覧回数
panchogalactico
Contributor II

I make it work, so I post here the answer.

If I set DMA_TCDn_SOFF = 0 , then the source pointer wont increment.

very easy actually.

0 件の賞賛
返信