Use VOUT33 to power other devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use VOUT33 to power other devices

1,485 Views
thiagopalmieri
Contributor III

Hello,

Can I use the VOUT33 pin to power other devices? It seems that it is pretty stable under 120mA and my board should be using far less than that.

If I have a dual power source option (5V via USB/VREGIN, or 3.3V from elsewhere) but only one of then will remain active at a given time (user choice), can I connect the VOUT33 and the 3.3V straight to each other without damaging the MCU? Maybe adding a schottky between them? I am using a KL43 chip.

Thx

Labels (2)
0 Kudos
Reply
1 Reply

1,329 Views
david_diaz
NXP Employee
NXP Employee

Hello Thiago,

Indeed, you can use the VOUT33 to power another devices.

Provided that you adhere to the USB VREG electrical specifications mentioned on the KL43 datasheet​, there will be no problems with the LPO from the USB regulator.

In this case the maximum output current the LPO can provide is up to 120 mA.

Please be aware that the external circuit is not demanding more than this current, 120 mA.

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply