Use RTC SG to wakeup MKL17 from LLS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use RTC SG to wakeup MKL17 from LLS

1,403 Views
daliagrimal
Contributor I

Hello,

 

I'm trying to wake a MKL17 from LLS on rtc sg if anyone here can be of help.

When I tryto wake a MKL17 from LLS on external pin, It is ok.

I'm setting bit 7 of the LLWU_ME to enable the RTC Sg as a wakeup module.

Labels (1)
0 Kudos
Reply
1 Reply

1,271 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Dalia Grimal

Are you able to share more information about your implementation? What is the source of the RTC? in some power modes the source clock could be powered off. Also, did you enable the RTC interruption? I would test the RTC functionality before enabling the power mode in the application.

For your reference:

http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf 

https://www.nxp.com/docs/en/application-note/AN5088.pdf 

Power Management on Kinetis MCUs: LLS and VLLS modes 

Also, I recommend the SDK code examples.

Best regards

0 Kudos
Reply