Use RTC SG to wakeup MKL17 from LLS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use RTC SG to wakeup MKL17 from LLS

1,445件の閲覧回数
daliagrimal
Contributor I

Hello,

 

I'm trying to wake a MKL17 from LLS on rtc sg if anyone here can be of help.

When I tryto wake a MKL17 from LLS on external pin, It is ok.

I'm setting bit 7 of the LLWU_ME to enable the RTC Sg as a wakeup module.

ラベル(1)
0 件の賞賛
返信
1 返信

1,313件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Dalia Grimal

Are you able to share more information about your implementation? What is the source of the RTC? in some power modes the source clock could be powered off. Also, did you enable the RTC interruption? I would test the RTC functionality before enabling the power mode in the application.

For your reference:

http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf 

https://www.nxp.com/docs/en/application-note/AN5088.pdf 

Power Management on Kinetis MCUs: LLS and VLLS modes 

Also, I recommend the SDK code examples.

Best regards

0 件の賞賛
返信