Update firmware and Erase and re-program a FRDM-KV31F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Update firmware and Erase and re-program a FRDM-KV31F

Update firmware and Erase and re-program a FRDM-KV31F

I have included the files needed to mass erase the flash of the MCU and re-program another binary.  

The procedure is shown in the folder " FRDM-KW31_FAT_added_2019"

Summarizing you...

1) update the debugger with bootloader mode (press reset and plug in usb cable) drag and drop .sda file on MSD bootloader.

2) unplug and re-plug USB. program the flashloader_loader_mkv31f512.bin by dragging and dropping the binary on to the virtual mass storage device FRDM-KV31 which appear when you plug the USB cable from the FRDM-KV31 to the PC. 

3) Open a CMD prompt window and navigate to the folder the files were unzipped to.

4) Determine the COM port by using the device manager

5) from the CMD prompt run the batch file 
    Erase_KMS_program_bubble.bat COMX

附件
无评分
版本历史
最后更新:
‎09-03-2019 02:36 PM
更新人: