Unable to Flash code in KEA-128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Flash code in KEA-128

1,892件の閲覧回数
vignesh_vb_7
Contributor IV

Hi,

I tried flashing my code by both Open-SDA and J--link segger.But i am unable to flash my code.

It is showing me an error message like this when i flashed my code with J-link Segger

ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory.

It is showing me an error message like this when i flashed my code with Open-SDA

ARM GDI Protocol Adapter : Can't connect. The Debugger can not connect to the P&E device

Can anyone tell me what is the problem and how to solve this ?

0 件の賞賛
返信
3 返答(返信)

1,718件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vignesh,

Which IDE do you used ?

Could you please send me the screenshot of the configuration when debug.

And i recommend you first create one simple project , then try to debug , check whether it can work well .

BR

Alice

0 件の賞賛
返信

1,718件の閲覧回数
vignesh_vb_7
Contributor IV

IMG_20151103_160828989[1].jpgIMG_20151103_160844316[1].jpgHi Alice,

I am using Code Warrior IDE

I tried a very simple program makiing a GPIO as high.It didn't work.

I hav attached the code and the pictures of it

0 件の賞賛
返信

1,718件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I have test your project on my side , it can work well.

Please select segger J-link, like this :

pastedImage_0.png

You can it can work well on my side :

pastedImage_1.png

Hope it helps



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,
Alice

0 件の賞賛
返信