USB0_DP and USB0_DM when USB not used - K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB0_DP and USB0_DM when USB not used - K60

ソリューションへジャンプ
3,287件の閲覧回数
igw
Contributor II

On a K60F what should we do with the USB0_DP and USB0_DM pins when we aren't using the USB peripheral?

There doesn't seem to be any guidance in the datasheet or user manual.

I was thinking that we would pull them down to GND lightly.  Or should we pull them up lightly?

Thanks,

Ian

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,950件の閲覧回数
wenlongzhang
Contributor II

just put both of them to GND is OK.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,951件の閲覧回数
wenlongzhang
Contributor II

just put both of them to GND is OK.

0 件の賞賛
返信
2,950件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ian,

Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.

It's ok to pull the USB0_DP and USB0_DM pins down to GND.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------