USB0_DP and USB0_DM when USB not used - K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB0_DP and USB0_DM when USB not used - K60

Jump to solution
2,138 Views
igw
Contributor II

On a K60F what should we do with the USB0_DP and USB0_DM pins when we aren't using the USB peripheral?

There doesn't seem to be any guidance in the datasheet or user manual.

I was thinking that we would pull them down to GND lightly.  Or should we pull them up lightly?

Thanks,

Ian

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,801 Views
wenlongzhang
Contributor II

just put both of them to GND is OK.

View solution in original post

0 Kudos
Reply
2 Replies
1,802 Views
wenlongzhang
Contributor II

just put both of them to GND is OK.

0 Kudos
Reply
1,801 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ian,

Thank you very much for your focus on Freescale Kinetis product. I'm glad to provide service for you.

It's ok to pull the USB0_DP and USB0_DM pins down to GND.


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------