USB to SPI dongle source code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB to SPI dongle source code?

Jump to solution
2,729 Views
frevoredo
Contributor I

I'm using the USB to SPI dongle which comes with the PT200 dev kit, but I've blown the KL25Z128 device on the board. I've ordered a new one , but need the code to program it. Does anyone know where I can it?

0 Kudos
Reply
1 Solution
2,476 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Frank,

You can download the USB SPI Dongle program for the KL25Z from this link:

http://cache.nxp.com/files/soft_dev_tools/hardware_tools/evbs/KITPT2000-KL25Z-EVBS.zip

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,477 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Frank,

You can download the USB SPI Dongle program for the KL25Z from this link:

http://cache.nxp.com/files/soft_dev_tools/hardware_tools/evbs/KITPT2000-KL25Z-EVBS.zip

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply