USB secondary ISP bootloader for LPC11U68

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB secondary ISP bootloader for LPC11U68

USB secondary ISP bootloader for LPC11U68

USB secondary ISP bootloader for LPC11U68

 Overview

       A Secondary Bootloader (SBL) is a piece of code that allows a user application code to be downloaded using alternative channels other than the standard UART0 used by the internal bootloader (on chip). Possible secondary bootloaders can be written for USB, Ethernet, SPI, SSP, CAN, and even I/Os. The secondary bootloader utilizes IAP as a method to update the user’s application code.

       The internal bootloader is the firmware that resides in the microcontroller’s boot ROM block and is executed on power-up and resets. After the boot ROM’s execution, the secondary bootloader would be executed, which will then execute the user application.
     The purpose of this document is to use USB as an example for developing the secondary bootloader and the code was tested using the LPCXpresso 11U68 evaluation board.

      The MSCD presents easy integration with a PC‘s operating systems. This class allows the embedded system’s flash memory space be represented as a folder in Windows/Linux. The user can update the flash with the binary image using drag and drop, so the following sections will present a guideline for development and implementation of the USB secondary bootloader design, configuration, and test.

     USB secondary bootloader code is base on the USB Mass Storage Class demo. However in this application note, we do not attempt to explain how the Mass Storage Class is implemented.

pastedImage_2.png

Fig 1 LPCXpresso Board for LPC11U68

Setup file (sbl_config.h)

      This file configures the secondary bootloader. The user should change this according to their application.

      Some definitions and explanation:
MAX_USER_SECTOR – This parameter is device dependent. In a 256 KB device, it will be 29 sectors, however the size of the last 5 sectors become the 32 KB instead of the 4 KB, so in the application, MAX_USER_SECTOR chooses 23 (Fig 2).
CRP – Code Read Protection. This parameter allows select the desired CRP level. Choosing CRP3, the primary bootloader’s entry mechanism check will be bypassed. Fig 3 for CRP details.
pastedImage_6.png

Fig 2 Flash sectors in LPC11U68

pastedImage_10.png

Fig 3 Code Read Protection (CRP)

Secondary bootloader entry

       The boot sequence shown below is used when entering the secondary USB bootloader.

pastedImage_14.png

Fig 4

Using an entry pin

     The secondary USB bootloader will check the status of a GPIO pin to determine if it should enter into programming mode. This is the easiest way since no post processing is needed. And this secondary bootloader uses P0.16.

Automatic secondary bootloader entry

      If the secondary USB bootloader detects that no user application is present upon reset, it will automatically enter programming mode.

ISP entry disabled

    If the secondary USB bootloader detects that a user application has already been installed and that CRP is set to level 3, then it will not enter ISP mode.

Bootloader size

       Since the bootloader resides within user programmable flash, it should be designed as small as possible. The larger the secondary USB bootloader is the less flash space is available to the user application. By default, the USB bootloader has been designed to fit within the first two flash sectors (Sector 0-1) so that the user application can start from sector 2.

Code placement in flash

      The secondary bootloader is placed at the starting address 0x0 so that it will be executed by the LPC11U68 after reset. Flash programming is based on a sector-by-sector basis. This means that the code for
the user application should not be stored in any of the same flash sectors as the secondary bootloader and for efficient use of the flash space, the user application should be flashed into the next available empty sector after the bootloader.

       In the application, the start sector is 3 (0x0000_3000) which is used to store the user application code.

User application execution

       If the SW2 button is not depressed, the secondary bootloader will start the execution of the user application. Execution of the user application is performed by updating the stack pointer (SP) and program counter (PC) registers. The SP points to the new location where the user application has allocated the top of its stack .The PC on the other hand contains the location of the first executable instruction in the user application. From here on the CPU will continue normal execution and initializations specified on the user application. By default, the bootloader uses 2 flash sectors. Therefore, to utilize the remaining flash, the secondary bootloader will look for the user application at 0x00003000

Handing interrupts

     The LPC11U68 contains a NVIC (Nested Vectored Interrupt Controller) that handles all interrupts. When an interrupt occurs the processor uses the vector table to locate the address of the handler.

     On the LPC11U68 the vector table is located in the same area of flash memory as the secondary bootloader. The secondary bootloader is designed to be permanently resident in flash memory and therefore it is not possible to update the contents of the vector table every time a new application is downloaded.
      The Cortex-M3 core allows the vector table to be remapped; however this is not the case with the Cortex-M0. Because of this, the secondary bootloader has been designed to redirect the processor to the handler listed in a vector table located in the application area of flash memory, see Fig 5.

pastedImage_17.png

Fig 5

User application

      To execute the user application the secondary USB bootloader will load the new SP and PC values into their respective registers, allowing the CPU to execute the new code correctly. Therefore, the user application must be built so that it can run from that starting address. In the application, this address is 0x00003E00. So relocate the user application storage area by following corresponding IDE’s User Guide.

 Testing

 Creating the binary file     

       In this application, I build the demos_switch_blinky which is from the LPCOpen library to create the binary which is compatible with the secondary USB bootloader. The binary see Table 1.

08 04 00 10 B5 09 00 00 07 07 00 00 9B 09 00 00 00 00 00 00 00 00 00 00 00 00 00 00 A1 E1 FF EF 00 00 00 00 00 00 00 00 00 00 00 00 A7 09 00 00 00 00 00 00 00 00 00 00 E5 09 00 00 27 03 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 01 03 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E3 09 00 00 E1 09 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 38 B5 63 4C 25 68 28 07 07 D5 96 20 E0 60 61 48 00 78 00 28 01 D1 00 F0 F7 F8 20 68 0C 21 29 40 01 43 21 60 31 BD 38 B5 5A 4C A0 78 40 1C A0 70 C0 B2 65 28 34 DB 00 25 A5 70 20 78 00 28 2F D0 60 78 00 28 03 D0 02 28 16 D0 0A D3 20 E0 01 21 00 F0 CA F8 00 21 01 20 00 F0 C6 F8 00 21 02 20 13 E0 01 21 01 20 00 F0 BF F8 00 21 00 20 00 F0 BB F8 00 21 02 20 08 E0 01 21 00 F0 B5 F8 00 21 01 20 00 F0 B1 F8 00 21 01 20 00 F0 AD F8 00 E0 65 70 60 78 40 1C 60 70 C0 B2 03 28 00 DB 65 70 31 BD F8 B5 00 F0 36 F9 00 F0 C2 F8 3A 48 01 68 02 22 91 43 01 60 01 68 38 4A 0A 40 02 60 35 4F 01 20 38 70 36 48 00 68 0A 21 00 F0 2B F9 1E 21 00 F0 28 F9 40 1E 00 26 80 21 49 04 88 42 0C D2 30 49 48 60 30 48 02 68 12 02 12 0A C0 23 1B 06 13 43 03 60 8E 60 07 20 08 60 01 20 2B 49 08 60 23 4C 20 00 00 F0 18 F9 29 48 01 68 80 22 12 03 0A 43 02 60 20 68 01 21 01 43 21 60 20 68 01 21 88 43 20 60 20 68 80 21 88 43 20 60 A6 60 FA 20 80 00 60 60 20 68 40 21 01 43 21 60 20 68 80 21 01 43 21 60 20 68 80 20 80 04 1A 49 08 60 20 68 30 21 01 43 21 60 18 4D 28 78 00 28 12 D1 38 78 00 28 0E D0 00 21 00 20 00 F0 3E F8 00 21 01 20 00 F0 3A F8 00 21 02 20 00 F0 36 F8 FA 20 80 00 E0 60 3E 70 E8 7B 00 28 E6 D1 01 20 38 70 E3 E7 00 40 02 40 04 00 00 10 00 20 00 A0 FF FF FE FF 00 00 00 10 10 E0 00 E0 20 ED 00 E0 1C 80 04 40 14 82 04 40 00 E1 00 E0 01 00 00 A0 49 01 40 18 83 54 70 47 10 B5 32 4C 20 00 00 F0 BF F8 E1 21 49 02 20 00 00 F0 C7 F8 03 20 E0 60 81 20 A0 60 80 20 20 63 10 BD 00 00 03 28 00 DB 70 47 80 B5 01 23 4B 40 2D A1 0A 5C 2B A1 09 5C A0 20 00 06 FF F7 DC FF 01 BD 00 00 03 28 00 DB 70 47 10 B5 A0 21 09 06 24 A2 12 5C 92 00 89 18 8C 22 92 01 01 23 00 BF 21 A4 20 5C 83 40 8B 50 10 BD 00 00 F8 B5 FF F7 C7 FF A0 25 2D 06 28 00 00 F0 B6 F8 00 24 00 BF 18 A6 31 5D 88 00 28 18 80 22 92 01 80 18 00 BF 15 A2 12 5D 03 68 01 27 97 40 1F 43 07 60 01 23 28 00 FF F7 A9 FF 64 1C 03 2C EA DB F1 BD 00 00 80 B5 07 48 01 68 80 22 52 02 0A 43 02 60 19 22 0A A1 04 48 00 F0 98 F8 01 BD 00 00 00 80 00 40 80 80 04 40 00 40 04 40 80 B5 FF F7 E9 FF 00 F0 B1 F8 01 BD 02 02 02 00 11 10 12 00 00 03 81 00 00 04 81 00 00 05 81 00 00 08 81 00 00 09 81 00 00 0B 02 00 00 0C 02 00 00 0D 02 00 00 0E 02 00 00 12 81 00 00 13 81 00 00 17 01 00 01 09 01 00 01 0B 81 00 01 0E 81 00 01 14 82 00 01 15 82 00 01 16 81 00 01 17 82 00 01 1A 81 00 01 1B 81 00 01 1D 81 00 02 00 01 00 02 01 01 00 02 03 82 00 80 B5 00 F0 EF F8 01 49 08 60 01 BD 00 00 00 10 80 B5 03 4A 12 68 12 69 52 68 90 47 02 BD 00 00 F8 1F FF 1F 03 48 01 68 80 22 D2 05 0A 43 02 60 70 47 00 00 80 80 04 40 15 49 01 22 8A 61 0A 68 80 23 5B 01 13 43 0B 60 07 21 81 60 10 21 81 62 70 47 70 B5 04 00 0D 00 01 20 0E 49 08 60 00 F0 8F F8 06 00 29 01 FF F7 D3 FF 01 00 E0 68 80 22 02 43 E2 60 C8 B2 20 60 08 04 00 0E 60 60 E0 68 80 22 90 43 E0 60 30 00 FF F7 C2 FF 70 BD 00 00 80 80 04 40 98 80 04 40 02 48 01 68 40 22 0A 43 02 60 70 47 80 80 04 40 00 2A 00 D1 70 47 30 B4 0C 68 23 0C 25 0A E4 B2 00 2C 12 D0 02 2C 01 D0 0A D3 11 E0 ED B2 AC 00 04 19 02 2D 01 DB F4 25 00 E0 F0 25 63 51 07 E0 2D 06 AC 0D 04 19 23 66 02 E0 2D 06 AC 0D 03 51 09 1D 52 1E E0 D1 30 BC 70 47 FE E7 38 B5 20 20 00 F0 E8 F8 00 20 00 90 11 48 02 E0 00 99 49 1C 00 91 00 99 81 42 F9 DB 01 20 00 F0 1F F8 0D 48 01 68 01 24 03 22 91 43 21 43 01 60 80 20 00 F0 C7 F8 09 4D 23 20 28 60 80 20 00 F0 CB F8 68 68 C0 07 FC D5 2C 67 03 20 00 F0 10 F8 31 BD 00 00 C4 09 00 00 10 C0 03 40 08 80 04 40 42 49 FF E7 08 60 00 20 48 60 01 20 48 60 70 47 3F 49 F7 E7 43 A0 CA 05 12 0F 92 00 80 58 C9 06 C9 0E 49 1C 49 00 FF F7 49 FF 00 BD 00 B5 00 20 3B 49 03 22 8B 6E 13 40 11 D0 02 2B 11 D0 02 D3 03 2B 10 D0 00 BD 89 6B 0A 40 08 D0 01 2A 03 D0 03 2A 1A D1 31 48 00 E0 2F 48 00 68 00 BD 2D 48 00 BD C9 69 D6 E7 8B 6B 1A 40 08 D0 01 2A 03 D0 03 2A 05 D1 29 48 00 E0 27 48 00 68 00 E0 25 48 09 68 C9 06 C9 0E 49 1C 48 43 00 BD 00 00 00 00 10 B5 00 20 22 4C 03 21 A2 6E 0A 40 30 D0 02 2A 15 D0 21 D3 03 2A 2C D1 A2 6B 11 40 08 D0 01 29 03 D0 03 29 05 D1 19 48 00 E0 17 48 00 68 00 E0 14 48 21 68 C9 06 C9 0E 49 1C 48 43 19 E0 E1 69 14 A0 CA 05 12 0F 92 00 80 58 C9 06 C9 0E 49 1C 49 00 FF F7 EB FE 0C E0 A2 6B 11 40 08 D0 01 29 03 D0 03 29 05 D1 09 48 00 E0 07 48 00 68 00 E0 04 48 21 6F FF F7 DA FE 10 BD 00 00 40 80 04 40 70 80 04 40 00 1B B7 00 D0 09 00 00 D4 09 00 00 08 80 04 40 00 00 00 00 C0 27 09 00 90 05 10 00 C0 5C 15 00 F0 B3 1A 00 20 0B 20 00 00 9F 24 00 E0 32 29 00 C0 C6 2D 00 50 97 31 00 E0 67 35 00 70 38 39 00 00 09 3D 00 40 16 40 00 80 23 43 00 C0 30 46 00 0B 49 0A 68 10 43 09 4A 02 40 C8 20 00 02 10 43 08 60 70 47 06 49 0A 68 82 43 04 48 10 40 C8 22 12 02 02 43 0A 60 70 47 00 00 00 00 FF 25 00 00 38 82 04 40 70 B4 01 21 00 22 13 E0 04 68 00 1D 0C 42 02 D0 4D 46 6D 1E 64 19 22 60 24 1D 1B 1F 04 2B FA D2 25 00 9E 07 01 D5 22 80 AD 1C 0B 40 00 D0 2A 70 03 68 00 1D 00 2B E7 D1 70 BC 70 47 10 B5 07 49 79 44 18 31 06 4C 7C 44 16 34 04 E0 08 1D 0A 68 89 18 88 47 01 00 A1 42 F8 D1 10 BD 08 00 00 00 14 00 00 00 9D FF FF FF 08 00 00 00 00 00 00 10 00 00 00 00 00 F0 0B F8 00 28 01 D0 FF F7 DE FF 00 20 00 BF 00 BF FF F7 0C FD 00 F0 02 F8 01 20 70 47 80 B5 00 F0 02 F8 01 BD FE E7 07 46 38 46 00 F0 02 F8 FB E7 FE E7 20 21 09 03 26 31 18 20 AB BE F9 E7 01 48 80 47 01 48 00 47 D9 09 00 00 C5 09 00 00 00 BF 00 BF 00 BF 00 BF FF F7 D2 FF 00 1B B7 00 00 80 00 00 80 B5 FF F7 DF FD 01 BD FE E7 FE E7 FE E7

                                                   Table 1


Drag and drop the binary file

  1. Running the secondary bootloader, and connect a USB cable between the PC and the J3, see Fig 6;

pastedImage_24.png

Fig 6

  1. Drag and drop the binary file to the driver, see Fig 7;

pastedImage_27.png

   Fig 7

  • Review the values of the user application in the relative area , see Fig 8;

pastedImage_30.png

Fig 8

ラベル(1)
添付
%3CLINGO-SUB%20id%3D%22lingo-sub-1119767%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ELPC11U68%E7%94%A8USB%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAISP%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119767%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20center%3B%22%3E%3CSTRONG%20style%3D%22font-size%3A%2028.0pt%3B%22%3ELPC11U68%E7%94%A8USB%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAISP%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%3C%2FSTRONG%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId-381683535%22%20id%3D%22toc-hId-1303201781%22%3E%26nbsp%3BOverview%3C%2FH1%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%20(SBL)%20%E3%81%AF%E3%80%81%E5%86%85%E9%83%A8%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%20(%E3%82%AA%E3%83%B3%E3%83%81%E3%83%83%E3%83%97)%20%E3%81%A7%E4%BD%BF%E7%94%A8%E3%81%95%E3%82%8C%E3%82%8B%E6%A8%99%E6%BA%96%E3%81%AE%20UART0%20%E4%BB%A5%E5%A4%96%E3%81%AE%E3%83%81%E3%83%A3%E3%83%8D%E3%83%AB%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%20%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%81%A7%E3%81%8D%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E3%81%99%E3%82%8B%E3%82%B3%E3%83%BC%E3%83%89%E3%81%A7%E3%81%99%E3%80%82%E5%8F%AF%E8%83%BD%E3%81%AA%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%80%81USB%E3%80%81%E3%82%A4%E3%83%BC%E3%82%B5%E3%83%8D%E3%83%83%E3%83%88%E3%80%81SPI%E3%80%81SSP%E3%80%81CAN%E3%80%81%E3%81%95%E3%82%89%E3%81%AB%E3%81%AFI%20%2F%20O%E7%94%A8%E3%81%AB%E6%9B%B8%E3%81%8F%E3%81%93%E3%81%A8%E3%81%8C%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%81%AE%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E6%9B%B4%E6%96%B0%E3%81%99%E3%82%8B%E6%96%B9%E6%B3%95%E3%81%A8%E3%81%97%E3%81%A6IAP%E3%82%92%E5%88%A9%E7%94%A8%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%20%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%86%85%E9%83%A8%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%80%81%E3%83%9E%E3%82%A4%E3%82%AF%E3%83%AD%E3%82%B3%E3%83%B3%E3%83%88%E3%83%AD%E3%83%BC%E3%83%A9%E3%81%AE%E3%83%96%E3%83%BC%E3%83%88ROM%E3%83%96%E3%83%AD%E3%83%83%E3%82%AF%E3%81%AB%E5%B8%B8%E9%A7%90%E3%81%99%E3%82%8B%E3%83%95%E3%82%A1%E3%83%BC%E3%83%A0%E3%82%A6%E3%82%A7%E3%82%A2%E3%81%A7%E3%80%81%E9%9B%BB%E6%BA%90%E6%8A%95%E5%85%A5%E6%99%82%E3%81%A8%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%E6%99%82%E3%81%AB%E5%AE%9F%E8%A1%8C%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E3%83%96%E3%83%BC%E3%83%88ROM%E3%81%AE%E5%AE%9F%E8%A1%8C%E5%BE%8C%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%8C%E5%AE%9F%E8%A1%8C%E3%81%95%E3%82%8C%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E5%AE%9F%E8%A1%8C%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3CBR%20%2F%3E%20%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%E3%81%93%E3%81%AE%E3%83%89%E3%82%AD%E3%83%A5%E3%83%A1%E3%83%B3%E3%83%88%E3%81%AE%E7%9B%AE%E7%9A%84%E3%81%AF%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%82%92%E9%96%8B%E7%99%BA%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AE%E4%BE%8B%E3%81%A8%E3%81%97%E3%81%A6%20USB%20%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%A7%E3%81%82%E3%82%8A%E3%80%81%E3%82%B3%E3%83%BC%E3%83%89%E3%81%AF%20LPCXpresso%2011U68%20%E8%A9%95%E4%BE%A1%E3%83%9C%E3%83%BC%E3%83%89%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%83%86%E3%82%B9%E3%83%88%E3%81%95%E3%82%8C%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3EMSCD%E3%81%AF%E3%80%81PC%E3%81%AE%E3%82%AA%E3%83%9A%E3%83%AC%E3%83%BC%E3%83%86%E3%82%A3%E3%83%B3%E3%82%B0%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E3%81%A8%E7%B0%A1%E5%8D%98%E3%81%AB%E7%B5%B1%E5%90%88%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%81%AE%E3%82%AF%E3%83%A9%E3%82%B9%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81%E7%B5%84%E3%81%BF%E8%BE%BC%E3%81%BF%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E3%81%AE%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%83%A1%E3%83%A2%E3%83%AA%E7%A9%BA%E9%96%93%E3%82%92Windows%2FLinux%E3%81%AE%E3%83%95%E3%82%A9%E3%83%AB%E3%83%80%E3%81%A8%E3%81%97%E3%81%A6%E8%A1%A8%E7%8F%BE%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%81%AF%E3%83%89%E3%83%A9%E3%83%83%E3%82%B0%20%E3%82%A2%E3%83%B3%E3%83%89%20%E3%83%89%E3%83%AD%E3%83%83%E3%83%97%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%20%E3%82%A4%E3%83%A1%E3%83%BC%E3%82%B8%E3%81%A7%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%82%92%E6%9B%B4%E6%96%B0%E3%81%A7%E3%81%8D%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E6%AC%A1%E3%81%AE%E3%82%BB%E3%82%AF%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%81%AF%E3%80%81USB%20%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AE%E8%A8%AD%E8%A8%88%E3%80%81%E6%A7%8B%E6%88%90%E3%80%81%E3%81%8A%E3%82%88%E3%81%B3%E3%83%86%E3%82%B9%E3%83%88%E3%81%AE%E9%96%8B%E7%99%BA%E3%81%A8%E5%AE%9F%E8%A3%85%E3%81%AE%E3%82%AC%E3%82%A4%E3%83%89%E3%83%A9%E3%82%A4%E3%83%B3%E3%82%92%E7%A4%BA%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3EUSB%20%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AE%E3%82%B3%E3%83%BC%E3%83%89%E3%81%AF%E3%80%81USB%20Mass%20Storage%20Class%20%E3%81%AE%E3%83%87%E3%83%A2%E3%81%AB%E5%9F%BA%E3%81%A5%E3%81%84%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%E3%81%9F%E3%81%A0%E3%81%97%E3%80%81%E3%81%93%E3%81%AE%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%83%8E%E3%83%BC%E3%83%88%E3%81%A7%E3%81%AF%E3%80%81Mass%20Storage%E3%82%AF%E3%83%A9%E3%82%B9%E3%81%8C%E3%81%A9%E3%81%AE%E3%82%88%E3%81%86%E3%81%AB%E5%AE%9F%E8%A3%85%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%8B%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%81%AF%E8%AA%AC%E6%98%8E%E3%81%97%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_2.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_2.png%22%20style%3D%22width%3A%20404px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111665iFD7877E81BFD1609%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_2.png%22%20alt%3D%22pastedImage_2.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B31%20LPC11U68%E7%94%A8LPCXpresso%E3%83%9C%E3%83%BC%E3%83%89%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId--1425770928%22%20id%3D%22toc-hId--504252682%22%3E%E3%82%BB%E3%83%83%E3%83%88%E3%82%A2%E3%83%83%E3%83%97%20%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%20(sbl_config.h)%3C%2FH1%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%81%93%E3%81%AE%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%81%AF%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%82%92%E8%A8%AD%E5%AE%9A%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%81%AF%E3%80%81%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AB%E5%BF%9C%E3%81%98%E3%81%A6%E3%81%93%E3%82%8C%E3%82%92%E5%A4%89%E6%9B%B4%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%20%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%81%84%E3%81%8F%E3%81%A4%E3%81%8B%E3%81%AE%E5%AE%9A%E7%BE%A9%E3%81%A8%E8%AA%AC%E6%98%8E%3A%3CBR%20%2F%3E%3CSTRONG%3EMAX_USER_SECTOR%3C%2FSTRONG%3E%20%E2%80%93%20%E3%81%93%E3%81%AE%E3%83%91%E3%83%A9%E3%83%A1%E3%83%BC%E3%82%BF%E3%81%AF%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%AB%E3%82%88%E3%81%A3%E3%81%A6%E7%95%B0%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82256%20KB%20%E3%81%AE%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%A7%E3%81%AF%2029%20%E3%82%BB%E3%82%AF%E3%82%BF%E3%81%AB%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E6%9C%80%E5%BE%8C%E3%81%AE%205%20%E3%82%BB%E3%82%AF%E3%82%BF%E3%81%AE%E3%82%B5%E3%82%A4%E3%82%BA%E3%81%AF%204%20KB%20%E3%81%A7%E3%81%AF%E3%81%AA%E3%81%8F%2032%20KB%20%E3%81%AB%E3%81%AA%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%81%AF%20MAX_USER_SECTOR%2023%20%E3%82%92%E9%81%B8%E6%8A%9E%E3%81%97%E3%81%BE%E3%81%99%20(%E5%9B%B3%202)%E3%80%82%3CBR%20%2F%3E%3CSTRONG%3ECRP%3C%2FSTRONG%3E%20%E2%80%93%20%E3%82%B3%E3%83%BC%E3%83%89%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8A%E4%BF%9D%E8%AD%B7%E3%80%82%E3%81%93%E3%81%AE%E3%83%91%E3%83%A9%E3%83%A1%E3%83%BC%E3%82%BF%E3%81%AB%E3%82%88%E3%82%8A%E3%80%81%E7%9B%AE%E7%9A%84%E3%81%AECRP%E3%83%AC%E3%83%99%E3%83%AB%E3%82%92%E9%81%B8%E6%8A%9E%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82CRP3%20%E3%82%92%E9%81%B8%E6%8A%9E%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81%E3%83%97%E3%83%A9%E3%82%A4%E3%83%9E%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AE%E3%82%A8%E3%83%B3%E3%83%88%E3%83%AA%20%E3%83%A1%E3%82%AB%E3%83%8B%E3%82%BA%E3%83%A0%20%E3%83%81%E3%82%A7%E3%83%83%E3%82%AF%E3%81%8C%E3%83%90%E3%82%A4%E3%83%91%E3%82%B9%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82CRP%E3%81%AE%E8%A9%B3%E7%B4%B0%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%81%AF%E3%80%81%E5%9B%B33%E3%80%82%3CBR%20%2F%3E%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111664i5CDB8E4CFDDC3D26%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_6.png%22%20alt%3D%22pastedImage_6.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B32%20LPC11U68%E3%81%AE%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%82%BB%E3%82%AF%E3%82%BF%20%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111663i541346D98264158F%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_10.png%22%20alt%3D%22pastedImage_10.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B33%20%E3%82%B3%E3%83%BC%E3%83%89%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8A%E4%BF%9D%E8%AD%B7(CRP)%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId-1061741905%22%20id%3D%22toc-hId-1983260151%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%20%E3%82%A8%E3%83%B3%E3%83%88%E3%83%AA%3C%2FH1%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E4%BB%A5%E4%B8%8B%E3%81%AB%E7%A4%BA%E3%81%99%E3%83%96%E3%83%BC%E3%83%88%E3%82%B7%E3%83%BC%E3%82%B1%E3%83%B3%E3%82%B9%E3%81%AF%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAUSB%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AB%E5%85%A5%E3%82%8B%E3%81%A8%E3%81%8D%E3%81%AB%E4%BD%BF%E7%94%A8%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_14.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_14.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111662i22B56A35F33E0AF8%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_14.png%22%20alt%3D%22pastedImage_14.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B34%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId-1752303379%22%20id%3D%22toc-hId--1621145671%22%3E%3CSPAN%20style%3D%22color%3A%20windowtext%3B%20font-size%3A%2014.0pt%3B%22%3E%E3%82%A8%E3%83%B3%E3%83%88%E3%83%AA%20PIN%20%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAUSB%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AF%E3%80%81GPIO%E3%83%94%E3%83%B3%E3%81%AE%E3%82%B9%E3%83%86%E3%83%BC%E3%82%BF%E3%82%B9%E3%82%92%E3%83%81%E3%82%A7%E3%83%83%E3%82%AF%E3%81%97%E3%81%A6%E3%80%81%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%9F%E3%83%B3%E3%82%B0%E3%83%A2%E3%83%BC%E3%83%89%E3%81%AB%E5%85%A5%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8B%E3%81%8B%E3%81%A9%E3%81%86%E3%81%8B%E3%82%92%E5%88%A4%E6%96%AD%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%82%8C%E3%81%AF%E3%80%81%E5%BE%8C%E5%87%A6%E7%90%86%E3%81%8C%E4%B8%8D%E8%A6%81%E3%81%AA%E3%81%9F%E3%82%81%E3%80%81%E6%9C%80%E3%82%82%E7%B0%A1%E5%8D%98%E3%81%AA%E6%96%B9%E6%B3%95%E3%81%A7%E3%81%99%E3%80%82%E3%81%9D%E3%81%97%E3%81%A6%E3%80%81%E3%81%93%E3%81%AE%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AFP0.16%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId--55151084%22%20id%3D%22toc-hId-866367162%22%3E%3CSPAN%20style%3D%22color%3A%20windowtext%3B%20font-size%3A%2014.0pt%3B%22%3E%E8%87%AA%E5%8B%95%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%82%A8%E3%83%B3%E3%83%88%E3%83%AA%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20USB%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%80%81%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%E6%99%82%E3%81%AB%E3%83%A6%E3%83%BC%E3%82%B6%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E5%AD%98%E5%9C%A8%E3%81%97%E3%81%AA%E3%81%84%E3%81%93%E3%81%A8%E3%82%92%E6%A4%9C%E5%87%BA%E3%81%97%E3%81%9F%E5%A0%B4%E5%90%88%E3%80%81%E8%87%AA%E5%8B%95%E7%9A%84%E3%81%AB%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%9F%E3%83%B3%E3%82%B0%E3%83%A2%E3%83%BC%E3%83%89%E3%81%AB%E5%85%A5%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId--1862605547%22%20id%3D%22toc-hId--941087301%22%3E%3CSPAN%20style%3D%22color%3A%20windowtext%3B%20font-size%3A%2014.0pt%3B%22%3EISP%20%E3%82%A8%E3%83%B3%E3%83%88%E3%83%AA%E3%81%8C%E7%84%A1%E5%8A%B9%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20USB%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%8C%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E3%81%99%E3%81%A7%E3%81%AB%E3%82%A4%E3%83%B3%E3%82%B9%E3%83%88%E3%83%BC%E3%83%AB%E3%81%95%E3%82%8C%E3%80%81CRP%20%E3%81%8C%E3%83%AC%E3%83%99%E3%83%AB%203%20%E3%81%AB%E8%A8%AD%E5%AE%9A%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%93%E3%81%A8%E3%82%92%E6%A4%9C%E5%87%BA%E3%81%97%E3%81%9F%E5%A0%B4%E5%90%88%E3%80%81ISP%20%E3%83%A2%E3%83%BC%E3%83%89%E3%81%AB%E3%81%AF%E5%85%A5%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId--1873108651%22%20id%3D%22toc-hId--951590405%22%3E%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AE%E3%82%B5%E3%82%A4%E3%82%BA%3C%2FH1%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%9E%E3%83%96%E3%83%AB%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E5%86%85%E3%81%AB%E5%AD%98%E5%9C%A8%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E3%81%A7%E3%81%8D%E3%82%8B%E3%81%A0%E3%81%91%E5%B0%8F%E3%81%95%E3%81%8F%E8%A8%AD%E8%A8%88%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20USB%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%8C%E5%A4%A7%E3%81%8D%E3%81%84%E3%81%BB%E3%81%A9%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E4%BD%BF%E7%94%A8%E3%81%A7%E3%81%8D%E3%82%8B%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%82%B9%E3%83%9A%E3%83%BC%E3%82%B9%E3%81%AF%E5%B0%91%E3%81%AA%E3%81%8F%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%E3%81%A7%E3%81%AF%E3%80%81USB%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E6%9C%80%E5%88%9D%E3%81%AE%202%20%E3%81%A4%E3%81%AE%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%82%BB%E3%82%AF%E3%82%BF%20(%E3%82%BB%E3%82%AF%E3%82%BF%200-1)%20%E5%86%85%E3%81%AB%E5%8F%8E%E3%81%BE%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E8%A8%AD%E8%A8%88%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AF%E3%82%BB%E3%82%AF%E3%82%BF%202%20%E3%81%8B%E3%82%89%E9%96%8B%E5%A7%8B%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId-614404182%22%20id%3D%22toc-hId-1535922428%22%3E%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%81%A7%E3%81%AE%E3%82%B3%E3%83%BC%E3%83%89%E9%85%8D%E7%BD%AE%3C%2FH1%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AF%E3%80%81%E3%83%AA%E3%82%BB%E3%83%83%E3%83%88%E5%BE%8C%E3%81%ABLPC11U68%E3%81%AB%E3%82%88%E3%81%A3%E3%81%A6%E5%AE%9F%E8%A1%8C%E3%81%95%E3%82%8C%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E3%80%81%E9%96%8B%E5%A7%8B%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%200x0%20%E3%81%AB%E9%85%8D%E7%BD%AE%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%9F%E3%83%B3%E3%82%B0%E3%81%AF%E3%80%81%E3%82%BB%E3%82%AF%E3%82%BF%E3%83%BC%E3%81%94%E3%81%A8%E3%81%AB%E8%A1%8C%E3%82%8F%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%82%8C%E3%81%AF%E3%80%81%3CBR%20%2F%3E%20%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AF%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%A8%E5%90%8C%E3%81%98%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%82%BB%E3%82%AF%E3%82%BF%E3%81%AB%E4%BF%9D%E5%AD%98%E3%81%97%E3%81%A6%E3%81%AF%E3%81%AA%E3%82%89%E3%81%9A%E3%80%81%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%82%B9%E3%83%9A%E3%83%BC%E3%82%B9%E3%82%92%E5%8A%B9%E7%8E%87%E7%9A%84%E3%81%AB%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%AB%E3%81%AF%E3%80%81%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AE%E6%AC%A1%E3%81%AB%E4%BD%BF%E7%94%A8%E5%8F%AF%E8%83%BD%E3%81%AA%E7%A9%BA%E3%81%AE%E3%82%BB%E3%82%AF%E3%82%BF%E3%81%AB%E3%83%A6%E3%83%BC%E3%82%B6%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%82%92%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%20%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%81%AF%E3%80%81%E9%96%8B%E5%A7%8B%E3%82%BB%E3%82%AF%E3%82%BF%E3%83%BC%E3%81%AF%203%20(0x0000_3000)%20%E3%81%A7%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%20%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E6%A0%BC%E7%B4%8D%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E4%BD%BF%E7%94%A8%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId-1304965656%22%20id%3D%22toc-hId--2068483394%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%20color%3A%20windowtext%3B%22%3E%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E5%AE%9F%E8%A1%8C%3C%2FSPAN%3E%3C%2FH2%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3ESW2%20%E3%83%9C%E3%82%BF%E3%83%B3%E3%81%8C%E6%8A%BC%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%AA%E3%81%84%E5%A0%B4%E5%90%88%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E5%AE%9F%E8%A1%8C%E3%82%92%E9%96%8B%E5%A7%8B%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E5%AE%9F%E8%A1%8C%E3%81%AF%E3%80%81%E3%82%B9%E3%82%BF%E3%83%83%E3%82%AF%E3%83%9D%E3%82%A4%E3%83%B3%E3%82%BF(SP)%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%A8%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%A0%E3%82%AB%E3%82%A6%E3%83%B3%E3%82%BF(PC)%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%82%92%E6%9B%B4%E6%96%B0%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%A7%E8%A1%8C%E3%81%84%E3%81%BE%E3%81%99%E3%80%82SP%E3%81%AF%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%83%BB%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E3%82%B9%E3%82%BF%E3%83%83%E3%82%AF%E3%81%AE%E6%9C%80%E4%B8%8A%E4%BD%8D%E3%82%92%E5%89%B2%E3%82%8A%E5%BD%93%E3%81%A6%E3%81%9F%E6%96%B0%E3%81%97%E3%81%84%E5%A0%B4%E6%89%80%E3%82%92%E6%8C%87%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E4%B8%80%E6%96%B9%E3%80%81PC%E3%81%AB%E3%81%AF%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E6%9C%80%E5%88%9D%E3%81%AE%E5%AE%9F%E8%A1%8C%E5%8F%AF%E8%83%BD%E5%91%BD%E4%BB%A4%E3%81%AE%E5%A0%B4%E6%89%80%E3%81%8C%E5%90%AB%E3%81%BE%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%81%93%E3%81%8B%E3%82%89%E3%80%81CPU%E3%81%AF%E9%80%9A%E5%B8%B8%E3%81%AE%E5%AE%9F%E8%A1%8C%E3%81%A8%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E6%8C%87%E5%AE%9A%E3%81%95%E3%82%8C%E3%81%9F%E5%88%9D%E6%9C%9F%E5%8C%96%E3%82%92%E7%B6%9A%E8%A1%8C%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%E3%81%A7%E3%81%AF%E3%80%81%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%AF%202%20%E3%81%A4%E3%81%AE%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%82%BB%E3%82%AF%E3%82%BF%E3%83%BC%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%97%E3%81%9F%E3%81%8C%E3%81%A3%E3%81%A6%E3%80%81%E6%AE%8B%E3%82%8A%E3%81%AE%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%E3%82%92%E5%88%A9%E7%94%A8%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%20%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%82%92%E6%8E%A2%E3%81%97%E3%81%BE%E3%81%990x00003000%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId--502488807%22%20id%3D%22toc-hId-419029439%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%20color%3A%20windowtext%3B%22%3E%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%81%AE%E5%87%A6%E7%90%86%3C%2FSPAN%3E%3C%2FH2%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3ELPC11U68%E3%81%AB%E3%81%AF%E3%80%81%E3%81%99%E3%81%B9%E3%81%A6%E3%81%AE%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%82%92%E5%87%A6%E7%90%86%E3%81%99%E3%82%8BNVIC(Nested%20Vectored%20Interrupt%20Controller)%E3%81%8C%E5%90%AB%E3%81%BE%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%E5%89%B2%E3%82%8A%E8%BE%BC%E3%81%BF%E3%81%8C%E7%99%BA%E7%94%9F%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81%E3%83%97%E3%83%AD%E3%82%BB%E3%83%83%E3%82%B5%E3%81%AF%E3%83%99%E3%82%AF%E3%82%BF%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%83%8F%E3%83%B3%E3%83%89%E3%83%A9%E3%81%AE%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%E3%82%92%E7%89%B9%E5%AE%9A%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3ELPC11U68%E3%81%A7%E3%81%AF%E3%80%81%E3%83%99%E3%82%AF%E3%82%BF%20%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%E3%81%AF%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%A8%E5%90%8C%E3%81%98%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%83%A1%E3%83%A2%E3%83%AA%E3%81%AE%E9%A0%98%E5%9F%9F%E3%81%AB%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%83%A1%E3%83%A2%E3%83%AA%E3%81%AB%E6%B0%B8%E7%B6%9A%E7%9A%84%E3%81%AB%E5%B8%B8%E9%A7%90%E3%81%99%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E8%A8%AD%E8%A8%88%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%81%9F%E3%82%81%E3%80%81%E6%96%B0%E3%81%97%E3%81%84%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%8C%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%81%95%E3%82%8C%E3%82%8B%E3%81%9F%E3%81%B3%E3%81%AB%E3%83%99%E3%82%AF%E3%83%88%E3%83%AB%20%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%E3%81%AE%E5%86%85%E5%AE%B9%E3%82%92%E6%9B%B4%E6%96%B0%E3%81%99%E3%82%8B%E3%81%93%E3%81%A8%E3%81%AF%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3CBR%20%2F%3E%20%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3BCortex-M3%E3%82%B3%E3%82%A2%E3%81%A7%E3%81%AF%E3%80%81%E3%83%99%E3%82%AF%E3%83%88%E3%83%AB%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%E3%82%92%E5%86%8D%E3%83%9E%E3%83%83%E3%83%94%E3%83%B3%E3%82%B0%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%E3%81%9F%E3%81%A0%E3%81%97%E3%80%81Cortex-M0%20%E3%81%AE%E5%A0%B4%E5%90%88%E3%81%AF%E3%81%9D%E3%81%86%E3%81%A7%E3%81%AF%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%E3%81%93%E3%81%AE%E3%81%9F%E3%82%81%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%20%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E3%80%81%E3%83%95%E3%83%A9%E3%83%83%E3%82%B7%E3%83%A5%20%E3%83%A1%E3%83%A2%E3%83%AA%E3%81%AE%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E9%A0%98%E5%9F%9F%E3%81%AB%E3%81%82%E3%82%8B%E3%83%99%E3%82%AF%E3%83%88%E3%83%AB%20%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%E3%81%AB%E3%83%AA%E3%82%B9%E3%83%88%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%83%8F%E3%83%B3%E3%83%89%E3%83%A9%E3%81%AB%E3%83%97%E3%83%AD%E3%82%BB%E3%83%83%E3%82%B5%E3%82%92%E3%83%AA%E3%83%80%E3%82%A4%E3%83%AC%E3%82%AF%E3%83%88%E3%81%99%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E8%A8%AD%E8%A8%88%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%20(%E5%9B%B3%205%20%E3%82%92%E5%8F%82%E7%85%A7)%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_17.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_17.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111661i07C2628212891FB1%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_17.png%22%20alt%3D%22pastedImage_17.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B35%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId--765256250%22%20id%3D%22toc-hId-156261996%22%3E%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BB%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%3C%2FH1%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAUSB%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%81%AF%E6%96%B0%E3%81%97%E3%81%84SP%E3%81%A8PC%E3%81%AE%E5%80%A4%E3%82%92%E3%81%9D%E3%82%8C%E3%81%9E%E3%82%8C%E3%81%AE%E3%83%AC%E3%82%B8%E3%82%B9%E3%82%BF%E3%81%AB%E3%83%AD%E3%83%BC%E3%83%89%E3%81%97%E3%80%81CPU%E3%81%8C%E6%96%B0%E3%81%97%E3%81%84%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E6%AD%A3%E3%81%97%E3%81%8F%E5%AE%9F%E8%A1%8C%E3%81%A7%E3%81%8D%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%97%E3%81%9F%E3%81%8C%E3%81%A3%E3%81%A6%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%83%BB%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AF%E3%80%81%E3%81%9D%E3%81%AE%E9%96%8B%E5%A7%8B%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%E3%81%8B%E3%82%89%E5%AE%9F%E8%A1%8C%E3%81%A7%E3%81%8D%E3%82%8B%E3%82%88%E3%81%86%E3%81%AB%E6%A7%8B%E7%AF%89%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%81%AF%E3%80%81%E3%81%93%E3%81%AE%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%E3%81%AF0x00003E00%E3%81%A7%E3%81%99%E3%80%82%E3%81%9D%E3%81%AE%E3%81%9F%E3%82%81%E3%80%81%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E3%82%B9%E3%83%88%E3%83%AC%E3%83%BC%E3%82%B8%E9%A0%98%E5%9F%9F%E3%82%92%E5%86%8D%E9%85%8D%E7%BD%AE%E3%81%99%E3%82%8B%E3%81%AB%E3%81%AF%E3%80%81%E5%AF%BE%E5%BF%9C%E3%81%99%E3%82%8BIDE%E3%81%AE%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%AC%E3%82%A4%E3%83%89%E3%81%AB%E5%BE%93%E3%81%A3%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CH1%20style%3D%22margin-left%3A%20.5in%3B%20text-indent%3A%20-.25in%3B%22%20id%3D%22toc-hId-1722256583%22%20id%3D%22toc-hId--1651192467%22%3E%E3%83%86%E3%82%B9%E3%83%86%E3%82%A3%E3%83%B3%E3%82%B0%3C%2FH1%3E%3CH2%20id%3D%22toc-hId-43884839%22%20id%3D%22toc-hId-965403085%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%20color%3A%20windowtext%3B%22%3E%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%81%AE%E4%BD%9C%E6%88%90%20%3C%2FSPAN%3E%3C%2FH2%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%81%93%E3%81%AE%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%A7%E3%81%AF%E3%80%81LPCOpen%E3%83%A9%E3%82%A4%E3%83%96%E3%83%A9%E3%83%AA%E3%81%8B%E3%82%89%E3%81%AEdemos_switch_blinky%E3%82%92%E3%83%93%E3%83%AB%E3%83%89%E3%81%97%E3%81%A6%E3%80%81%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AAUSB%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%81%A8%E4%BA%92%E6%8F%9B%E6%80%A7%E3%81%AE%E3%81%82%E3%82%8B%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%82%92%E4%BD%9C%E6%88%90%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%81%AF%E8%A1%A8%201%20%E3%82%92%E5%8F%82%E7%85%A7%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CTABLE%20style%3D%22border%3A%20none%3B%22%3E%3CTBODY%3E%3CTR%3E%3CTD%20style%3D%22border%3A%20solid%20%237295D2%201.0pt%3B%20background%3A%20%23D0DBF0%3B%20padding%3A%200in%205.4pt%200in%205.4pt%3B%22%20width%3D%22590%22%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20center%3B%22%3E%3CSTRONG%20style%3D%22font-size%3A%2012.0pt%3B%22%3E08%2004%2000%2010%20B5%2009%2000%2000%2007%2007%2000%2000%209B%2009%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%20A1%20E1%20FF%20EF%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%20A7%2009%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%2000%20E5%2009%2000%2000%2000%2027%2003%2000%2000%20E3%2009%2000%2000%20E3%2009%200000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E300%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%2001%2003%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E3%2009%2000%2000%20E1%2009%2000%2000%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FF%20FFFF%20FF%2038%20B5%2063%204C%2025%2068%2028%2007%20D5%2096%2020%20E0%2060%2061%2041%2048%2000%2078%2000%2028%2001%20D1%2000%20F0%20F7%20F8%2020%2068%200C%2021%2029%204001%2043%2021%2060%2031%20BD%2038%20B5%205A%204C%20A0%2078%2040%201C%20A0%2070%20C0%20B2%2065%2028%2034%20DB%2000%2025%20A5%2070%2020%2078%2000%2028%202F%20D0%2060%2078%2000%2028%2003%20D0%2002%2028%2016%20D0%200A%20D3%2020%20E0%2001%2021%2000%20F0%20CA%20F8%2000%2021%2001%2020%2000%20F0%20C6%20F8%2000%2021%2002%2020%2013%20E0%2001%2021%2001%2020%2000%20F0%20BF%20F8%200021%2000%2020%2000%20F0%20BB%20F8%2000%2021%2002%2020%2008%20E0%2001%2021%2000%20F0%20B5%20F8%2000%2021%2001%2020%2000%20F0%20B1%20F8%2000%2021%2001%2020%2000%20F0%20AD%20F8%2000%20E0%2065%2070%2060%2078%2040%201C%2060%2070%20C0%20B2%2003%2028%2000%20DB%2065%2070%2031%20BD%20F8%20B5%2000%20F0%2036%20F9%2000%20F0%20C2%20F8%203A%2048%2001%2068%2002%2022%2091%2043%2001%206001%2068%2038%204A%200A%2040%2002%2060%2035%204F%2001%2020%2038%2070%2036%2048%2000%2068%200A%2021%2000%20F0%202B%20F9%201E%2021%2000%20F0%2028%20F9%2040%201E%2000%2026%2080%2021%2049%2004%2088%2042%200C%20D2%2030%2049%2048%2060%2030%2048%2002%2068%2012%2002%2012%200A%20C0%2023%201B%2006%2013%2043%2003%2060%208E%2060%2007%2020%2008%2060%2001%2020%202B%2049%2008%2060%2023%204C%2020%2000%2000%20F0%2018%20F9%2029%2048%2001%2068%2080%2022%2012%2003%200A%2043%2002%2060%2020%2068%2001%2021%2001%2043%2021%2060%2020%2068%2001%2021%2088%2043%2020%2060%2020%2068%2080%2021%2088%2043%2020%2060%2060%20A6%2060%20FA%2020%2080%2000%206060%2020%2068%2040%2021%2001%2043%2021%2060%2020%2068%2080%2021%2001%2043%2021%2060%2020%2068%2080%2020%2080%2004%201A%2049%2008%2060%2020%2068%2030%2021%2001%2043%2021%2060%2018%204D%2028%2078%2000%2028%2012%20D1%2038%2078%2000%2028%200E%20D0%2000%2021%2000%2020%2000%20F0%203E%20F8%2000%2021%2001%2020%2000%20F0%203A%20F8%2000%2021%2002%2020%2000%20F0%2036%20F8%20FA%202080%2000%20E0%2060%203E%2070%20E8%207B%2000%2028%20E6%20D1%2001%2020%2038%2070%20E3%20E7%2000%2040%2002%2040%2004%2000%2000%2010%2000%2020%2000%20A0%20FF%20FF%20FE%20FF%2000%2000%2000%2010%2010%20E0%2000%20E0%2020%20ED%2000%20E0%201C%2080%2004%2040%2014%2082%2004%2004%2040%2000%20E1%2000%20E0%2001%2000%2000%20A0%2049%2001%2040%2018%2083%2054%2070%2047%2010%20B5%2032%204C%202000%2000%20F0%20BF%20F8%20E1%2021%2049%2002%2020%2000%2000%20F0%20C7%20F8%2003%2020%20E0%2060%2081%2020%20A0%2060%2080%2020%2020%2063%2010%20BD%2000%2000%2003%2028%2000%20DB%2070%2047%2080%20B5%2001%2023%204B%2040%202D%20A1%200A%205C%202B%20A1%2009%205C%20A0%2020%2000%2006%20FF%20F7%20DC%20FF%2001%20BD%2000%2000%2003%2028%2000%20DB%2070%2047%2010%20B5%20A0%2021%2009%200624%20A2%2012%205C%2092%2000%2089%2018%208C%2022%2092%2001%2001%2023%2000%20BF%2021%20A4%2020%205C%2083%2040%208B%2050%2010%20BD%2000%2000%20F8%20B5%20FF%20F7%20C7%20FF%20A0%2025%202D%2006%2028%2000%2000%20F0%20B6%20F8%2000%2024%2000%20BF%2018%20A6%2031%205D%2088%2000%2028%2018%2080%2022%2092%2001%2080%2018%2000%20BF%2015%20A2%2012%205D%2003%2068%2001%2027%2097%2040%201F43%2007%2060%2001%2023%2028%2000%20FF%20F7%20A9%20FF%2064%201C%2003%202C%20EA%20DB%20F1%20BD%2000%2000%2080%20B5%2007%2048%2001%2068%2080%2022%2052%2002%200A%2043%2002%2060%2019%2022%200A%20A1%2004%2048%2000%20F0%2098%20F8%2001%20BD%2000%2000%2000%2000%2080%2000%2040%2080%2080%2004%2040%2000%2040%2080%2080%20B5%20FF%20F7%20E9%20FF%2000%20F0%20B1%20F8%2001%20BD%2002%200202%2000%2011%2010%2012%2000%2000%2003%2081%2000%2000%2004%2081%2000%2000%2005%2081%2000%2000%2008%2081%2000%2000%2009%2081%2000%2000%200B%2002%2000%2000%200C%2002%2000%2000%200D%2002%2000%2000%200E%2002%2000%2000%2012%2081%2000%2000%2013%2081%2000%2000%2017%2001%2000%2001%2009%2001%2000%2001%200B%2081%2000%2001%200E%2081%2000%2001%2014%2082%2000%2001%2015%2082%2000%2001%2016%2081%2000%2001%2017%2082%2000%2001%201A%2081%2000%2001%201B%2081%2000%2001%201D%2081%2000%2002%2000%2001%2000%2002%2001%2001%2000%2002%2003%2082%2000%2080%20B5%2000%20F0%20EF%20F8%2001%2049%2008%2060%2001%20BD%2000%2000%2000%2010%2080%20B5%20034A%2012%2068%2012%2069%2052%2068%2090%2047%2002%20BD%2000%2000%20F8%201F%20FF%201F%2003%2048%2001%2068%2080%2022%20D2%2005%200A%2043%2002%2060%2070%2047%2000%2000%2080%2080%2004%2040%2015%2049%2001%2022%208A%2061%200A%2068%2080%2023%205B%2001%2013%2043%200B%2060%2007%2021%2081%2060%2010%2021%2062%2070%2047%2070%20B5%2004%2000%200D%2000%2001%2020%200E%2049%2008%206000%20F0%208F%20F8%2006%2000%2029%2001%20FF%20F7%20D3%20FF%2001%2000%20E0%2068%2080%2022%2002%2043%20E2%2060%20C8%20B2%2020%2060%2008%2004%2000%200E%2060%2060%20E0%2068%2080%2022%2090%2043%20E0%2060%2030%2000%20FF%20F7%20C2%20FF%2070%20BD%2000%2000%2080%2080%2004%2040%2098%2080%2004%2040%2002%2048%2001%2068%2040%2022%200A%2043%2002%2070%2047%2080%2080%2004%2040%20002A%2000%20D1%2070%2047%2030%20B4%200C%2068%2023%200C%2025%200A%20E4%20B2%2000%202C%2012%20D0%2002%202C%2001%20D0%200A%20D3%2011%20E0%20ED%20B2%20AC%2000%2004%2019%2002%202D%2001%20DB%20F4%2025%2000%20E0%20F0%2025%2063%2051%2007%20E0%202D%2006%20AC%200D%2004%2019%2023%2066%2002%20E0%202D%2006%20AC%200D%2003%2051%2009%201D%2052%201E%20E0%20D1%2030%20BC%2070%2047%20FE%20E738%20B5%2020%2020%2000%20F0%20E8%20F8%2000%2020%2000%2090%2011%2048%2002%20E0%2000%2099%2049%201C%2000%2091%2000%2099%2081%2042%20F9%20DB%2001%2020%2000%20F0%201F%20F8%200D%2048%2001%2068%2001%2024%2003%2022%2091%2043%2021%2043%2001%2060%2080%2020%2000%20F0%20C7%20F8%2009%204D%2023%2020%2028%2060%2080%2020%2000%20F0%20CB%20F8%2068%2068%20C0%2007%20FC%20D5%202C%2067%200320%2000%20F0%2010%20F8%2031%20BD%2000%2000%20C4%2009%2000%2000%2010%20C0%2003%2040%2008%2080%2004%2040%2042%2049%20FF%20E7%2008%2060%2000%2020%2048%2060%2001%2020%2048%2060%2070%2047%203F%2049%20F7%20E7%2043%20A0%20CA%2005%2012%200F%2092%2000%2080%2058%20C9%2006%20C9%200E%2049%201C%2049%2000%20FF%20F7%2049%20FF%2000%20BD%2000%20B5%2000%2020%203B%2049%2003%2022%208B%206E13%2040%2011%20D0%2002%202B%2011%20D0%2002%20D3%2003%202B%2010%20D0%2000%20BD%2089%206B%200A%2040%2008%20D0%2001%202A%2003%20D0%2003%202A%201A%20D1%2031%2048%2000%20E0%202F%2048%2000%2068%2000%20BD%202D%2048%2000%20BD%20C9%2069%20D6%20E7%208B%206B%201A%2040%2008%20D0%2001%202A%2003%20D0%2003%202A%2005%20D1%2029%2048%2000%20E0%2027%2048%2000%2068%2000%20E0%2025%2048%2009%2068%20C9%2006%20C9%200E%2049%201C%2048%2043%2000%20BD%2000%2000%2000%2000%2010%20B5%2000%2020%2022%204C%2003%2021%20A2%206E%200A%2040%2030%20D0%2002%202A%2015%20D0%2021%20D3%2003%202A%202C%20D1%20A2%206B%2011%2040%2008%20D0%2001%2029%2003%20D0%200329%2005%20D1%2019%2048%2000%20E0%2017%2048%2000%2068%2000%20E0%2014%2048%2021%2068%20C9%2006%20C9%200E%2049%201C%2048%2043%2019%20E0%20E1%2069%2014%20A0%20CA%2005%2012%200F%2092%2000%2080%2058%20C9%2006%20C9%200E%2049%201C%2049%2000%20FF%20F7%20EB%20FE%200C%20E0%20A2%206B%2011%2040%2008%20D0%2001%2029%2003%20D0%2003%2029%2005%20D1%2009%2048%2000%20E0%2007%2048%2000%206800%20E0%2004%2048%2021%206F%20FF%20F7%20DA%20FE%2010%20BD%2000%2000%2040%2080%2004%2040%2070%2080%2004%2040%2000%201B%20B7%2000%20D0%2009%2000%2000%20D4%2009%2000%2000%2008%2080%2004%2040%2000%2000%2000%2000%20C0%2027%2009%2000%2090%2005%2010%2000%20C0%205C%2015%2000%20F0%20B3%201A%2000%2020%200B%2020%2000%2000%209F%2024%2000%20E0%2032%2029%2000%20C0%20C6%202D%2000%205097%2031%2000%20E0%2067%2035%2000%2070%2038%2039%2000%2000%2009%203D%2000%2040%2016%2040%2000%2080%2023%2043%2000%20C0%2030%2046%2000%200B%2049%200A%2068%2010%2043%2009%204A%2002%2040%20C8%2020%2000%2002%2010%2043%2008%2060%2070%2047%2006%2049%200A%2068%2082%2043%2004%2048%2010%2040%20C8%2022%2012%2002%2002%2043%200A%2060%2070%2047%2000%2000%2000%20FF%2025%2000%200038%2082%2004%2040%2070%20B4%2001%2021%2000%2022%2013%20E0%2004%2068%2000%201D%200C%2042%2002%20D0%204D%2046%206D%201E%2064%2019%2022%2060%2024%201D%201B%201F%2004%202B%20FA%20D2%2025%2000%209E%2007%2001%20D5%2022%2080%20AD%201C%200B%2040%2000%20D0%202A%2070%2003%2068%2000%201D%2000%202B%20E7%20D1%2070%20BC%2070%2047%2010%20B5%2007%2049%2079%2044%2018%2031%2006%204C%207C44%2016%2034%2004%20E0%2008%201D%200A%2068%2089%2018%2088%2047%2001%2000%20A1%2042%20F8%20D1%2010%20BD%2008%2000%2000%2000%2014%2000%2000%2000%209D%20FF%20FF%20FF%20FF%2008%2000%2000%2000%2000%2000%2000%2000%2010%2000%2000%2000%2000%2000%20F0%200B%20F8%2000%2028%2001%20D0%20FF%20F7%20DE%20FF%2000%2020%2000%20BF%2000%20BF%20FF%20F7%200C%20FD%2000%20F0%2002%20F8%2001%2020%2070%204780%20B5%2000%20F0%2002%20F8%2001%20BD%20FE%20E7%2007%2046%2038%2046%2000%20F0%2002%20F8%20FB%20E7%20FE%20E7%2020%2021%2009%2003%2026%2031%2018%2020%20AB%20BE%20F9%20E7%2001%2048%2080%2047%2001%2048%2000%2047%20D9%2009%2000%2000%20C5%2009%2000%2000%2000%20BF%2000%20BF%2000%20BF%2000%20BF%20FF%20F7%20D2%20FF%2000%201B%20B7%2000%2000%2080%2000%2000%2080%20B5%20FF%20F7%20DF%20FD%2001%20BD%20FE%20E7%20FE%20E7%20FE%20E7%20FE%20E7%3C%2FSTRONG%3E%3C%2FP%3E%3C%2FTD%3E%3C%2FTR%3E%3C%2FTBODY%3E%3C%2FTABLE%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%83%86%E3%83%BC%E3%83%96%E3%83%AB%201%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CBR%20%2F%3E%20%3C%2FSPAN%3E%3C%2FP%3E%3CH2%20id%3D%22toc-hId--1763569624%22%20id%3D%22toc-hId--842051378%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%20color%3A%20windowtext%3B%22%3E%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%82%92%E3%83%89%E3%83%A9%E3%83%83%E3%82%B0%E3%82%A2%E3%83%B3%E3%83%89%E3%83%89%E3%83%AD%E3%83%83%E3%83%97%E3%81%97%E3%81%BE%E3%81%99%3C%2FSPAN%3E%3C%2FH2%3E%3COL%3E%3CLI%20style%3D%22text-indent%3A%20-.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%20%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%82%BB%E3%82%AB%E3%83%B3%E3%83%80%E3%83%AA%E3%83%96%E3%83%BC%E3%83%88%E3%83%AD%E3%83%BC%E3%83%80%E3%83%BC%E3%82%92%E5%AE%9F%E8%A1%8C%E3%81%97%E3%80%81PC%E3%81%A8J3%E3%81%AE%E9%96%93%E3%81%ABUSB%E3%82%B1%E3%83%BC%E3%83%96%E3%83%AB%E3%82%92%E6%8E%A5%E7%B6%9A%E3%81%97%E3%81%BE%E3%81%99(%E5%9B%B36%E3%82%92%E5%8F%82%E7%85%A7)%E3%80%82%3C%2FSPAN%3E%3C%2FLI%3E%3C%2FOL%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_24.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_24.png%22%20style%3D%22width%3A%20545px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111660iF8351AAC3E42C387%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_24.png%22%20alt%3D%22pastedImage_24.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B36%3C%2FSPAN%3E%3C%2FP%3E%3COL%3E%3CLI%20style%3D%22text-indent%3A%20-.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%20%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E3%83%90%E3%82%A4%E3%83%8A%E3%83%AA%E3%83%95%E3%82%A1%E3%82%A4%E3%83%AB%E3%82%92%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%E3%81%AB%E3%83%89%E3%83%A9%E3%83%83%E3%82%B0%E3%82%A2%E3%83%B3%E3%83%89%E3%83%89%E3%83%AD%E3%83%83%E3%83%97%E3%81%97%E3%81%BE%E3%81%99(%E5%9B%B37%E3%82%92%E5%8F%82%E7%85%A7)%E3%80%82%3C%2FSPAN%3E%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_27.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_27.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F9143i2C11139A19044800%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_27.png%22%20alt%3D%22pastedImage_27.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B37%3C%2FSPAN%3E%3C%2FP%3E%3CUL%3E%3CLI%20style%3D%22text-indent%3A%20-.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%20%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E7%9B%B8%E5%AF%BE%E9%A0%98%E5%9F%9F%E3%81%A7%E3%83%A6%E3%83%BC%E3%82%B6%E3%83%BC%E3%82%A2%E3%83%97%E3%83%AA%E3%82%B1%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E5%80%A4%E3%82%92%E7%A2%BA%E8%AA%8D%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E5%9B%B38%E3%82%92%E5%8F%82%E7%85%A7%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FSPAN%3E%3C%2FLI%3E%3C%2FUL%3E%3CP%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_30.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_30.png%22%20style%3D%22width%3A%20580px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111659i154ED2153BE2C772%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_30.png%22%20alt%3D%22pastedImage_30.png%22%20%2F%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20center%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2012.0pt%3B%22%3E%E5%9B%B38%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1119767%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3EKinetis%20K%E3%82%B7%E3%83%AA%E3%83%BC%E3%82%BAMCU%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E
評価なし
バージョン履歴
最終更新日:
‎11-28-2016 06:40 PM
更新者: