USB host communication with more devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB host communication with more devices

ソリューションへジャンプ
1,866件の閲覧回数
Luky
Contributor II

Hi,

I will develop a new project and I need to communicate between one USB host device (maybe Kinetis K or KL) and more devices (8bit MC9S08JS16). Devices will connect to USB host over USB HUB. This is my idea. I haven´t had any experience with USB Stack yet. I need to know if it is possible. Thanks for the answer.

Lukas

0 件の賞賛
返信
1 解決策
1,750件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lukas,

I don't think your scheme could achieve.

Selecting a KL or K series MCU as the USB host device can handle the devices whose total number is based on the USB modules the USB host contains under without using the USB HUB.

In another word, if you want to the USB host device communicate with three or more devices, it can't work it out certainly.

Hope the reply helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,751件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lukas,

I don't think your scheme could achieve.

Selecting a KL or K series MCU as the USB host device can handle the devices whose total number is based on the USB modules the USB host contains under without using the USB HUB.

In another word, if you want to the USB host device communicate with three or more devices, it can't work it out certainly.

Hope the reply helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信