USB host MSD Hard Fault in K20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB host MSD Hard Fault in K20

1,520 次查看
carxander
Contributor II

The problem is as follows:

 

I adapted one of the examples to work with USB Stack Processor Expert, specifically "C:\Freescale\Freescale USB Stack v4.0.3\Source\Host\examples\msd_mfs_generic\cw10\kinetis_k20". I've checked the processor clock settings, I used the USB Host Stack component of the PE.

 

The way I adapted was creating a new project in PE and adding the libraries used in the example. I also put the pin PTC9 to 1 to enable the USB 5V.

 

Everything compiles, the USB get interface.

 

Mount the file system,

 

f_result = f_mount(HOST_CONTROLLER_NUMBER, &fatfs);

 

but when I try to open a file or do any "MFS" operation

 

f_result = f_open(&archivo, "/Test.txt", FA_READ);

 

I have a Hard Fault.

 

sometimes instead of a Hard Fault the program continues to run but the function f_mount returns error:

 

 

FR_DISK_ERR,/* (1) A hard error occured in the low level disk I/O layer */

 

That's related to "diskio.c"

 

I tried a PE component made by Erich Styger to trace HardFaults and trace the last executed code to a function in 'hostmain.c'.

 

I'm a little confused and don't know where to find.

 

Attached the source code to see if someone can give me a hand.

.

Sorry for spelling errors or syntax, (I do best reading in english than writing)

Original Attachment has been moved to: TestUSB-MSD.rar.zip

标签 (2)
0 项奖励
回复
0 回复数