USB Vregin input - MK64

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Vregin input - MK64

ソリューションへジャンプ
2,238件の閲覧回数
roymessinger
Contributor V

I'm designing a board based on the MK64 (the FRDM K64 is my reference design). I do not use the USB features of the MK64. I am using the UART capabilities (using USB dongle to RS485 cable from a far host PC to my controller board, then to UART inputs on the MK64 via a MAX3362 RS 485 Transceiver).

In such case, do I need to connect a voltage to that pin?

Leave it float?

Thanks!

0 件の賞賛
返信
1 解決策
2,062件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.

Unused analog interfaces.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,062件の閲覧回数
roymessinger
Contributor V

Ok.

Thank you very much!

I've posted another question regarding un used I/O's and output state at reset.

Can you amswer that also?

0 件の賞賛
返信
2,063件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.

Unused analog interfaces.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信