USB Vregin input - MK64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Vregin input - MK64

Jump to solution
2,240 Views
roymessinger
Contributor V

I'm designing a board based on the MK64 (the FRDM K64 is my reference design). I do not use the USB features of the MK64. I am using the UART capabilities (using USB dongle to RS485 cable from a far host PC to my controller board, then to UART inputs on the MK64 via a MAX3362 RS 485 Transceiver).

In such case, do I need to connect a voltage to that pin?

Leave it float?

Thanks!

0 Kudos
Reply
1 Solution
2,064 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.

Unused analog interfaces.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,064 Views
roymessinger
Contributor V

Ok.

Thank you very much!

I've posted another question regarding un used I/O's and output state at reset.

Can you amswer that also?

0 Kudos
Reply
2,065 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Roy,

Connect VREGIN and VOUT33 together and tie to ground through a 10kΩ resistor.

Unused analog interfaces.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply