USB Regulator in Host Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Regulator in Host Mode

跳至解决方案
1,581 次查看
TerryMcHenry
Contributor II

I would like to run the USB on a KL25 in host mode, so I don't need the on-chip linear regulator.  If I look in the reference manual, figure 36-2, I see that the regulator powers "other modules" and then goes to an output pin.  What are these "other modules"?  The ultimate question is, I have 3.3V available so I don't need the regulator, can I leave it unconnected or is there something internal to the chip that needs to be powered by the output of the regulator?

标签 (2)
标记 (3)
1 解答
1,474 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Terry:

The USB regulator provides power to the internal USB transceiver itself, so you cannot leave it unconnected. You may wire VREGIN to VDD in case you do not have another source, and also place the external 2.2 uF capacitor even if output voltage is not used.

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,474 次查看
TerryMcHenry
Contributor II

Perfect Jorge, thanks!

1,475 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Terry:

The USB regulator provides power to the internal USB transceiver itself, so you cannot leave it unconnected. You may wire VREGIN to VDD in case you do not have another source, and also place the external 2.2 uF capacitor even if output voltage is not used.

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复