USB Regulator in Host Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Regulator in Host Mode

Jump to solution
2,696 Views
TerryMcHenry
Contributor II

I would like to run the USB on a KL25 in host mode, so I don't need the on-chip linear regulator.  If I look in the reference manual, figure 36-2, I see that the regulator powers "other modules" and then goes to an output pin.  What are these "other modules"?  The ultimate question is, I have 3.3V available so I don't need the regulator, can I leave it unconnected or is there something internal to the chip that needs to be powered by the output of the regulator?

Labels (2)
1 Solution
2,589 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Terry:

The USB regulator provides power to the internal USB transceiver itself, so you cannot leave it unconnected. You may wire VREGIN to VDD in case you do not have another source, and also place the external 2.2 uF capacitor even if output voltage is not used.

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,589 Views
TerryMcHenry
Contributor II

Perfect Jorge, thanks!

2,590 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Terry:

The USB regulator provides power to the internal USB transceiver itself, so you cannot leave it unconnected. You may wire VREGIN to VDD in case you do not have another source, and also place the external 2.2 uF capacitor even if output voltage is not used.

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply