USB-MSD Boot Loader OS compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB-MSD Boot Loader OS compatibility

1,292件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

USB-MSD bootloaders have become very popular in the last few years but OS manufacturers are not always making life easy with their enhancements to the behavior when external hardware driver are connected - Windows 8.1 update added a well known tripping stone which doesn't allow older mbed loaders to operate correctly, or be updated to newer versions with workarounds, for instance.

However Windows 8.1 is almost harmless in comparison to MAC OS X.

The uTasker serial loader (including KBOOT compatibility and USB-MSD in parallel) and available for all K and KL devices with USB was of course also not saved a certain amount of agony to ensure compatibility. For the low-down on just what the MAC OS X does with SD cards and USB-MSD loaders and workarounds implemented see the following development story:

http://www.utasker.com/kinetis/USB-MSD-MAC.html

Regards

Mark

Kinetis: µTasker Kinetis support

For the complete "out-of-the-box" Kinetis experience and faster time to market

ラベル(3)
タグ(3)
0 件の賞賛
返信
0 返答(返信)