USB ISTAT register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB ISTAT register

1,356件の閲覧回数
James8
Contributor I

Hi, I seem to be having a problem clearing the flags in this register... I have read in the datasheet that they are cleared by writing a 1 to the bit, which is counter intuitive but nevermind, but when I do write a 1 (or a 0 for that matter) the register doesn't change, it appears to be read only.

 

I have tried to use several USB example projects (every one I could find), and none of them work, potentially because of this problem, they all rely on the flags being cleared and thus end up getting stuck in infinite loops etc.

 

Any ideas?

 

 

 

 

0 件の賞賛
返信
1 返信

1,246件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Writing 1 to the bit to be cleared is the technique that is used.

Check that the interrupt status register is declared as a byte wide register with volatile attributes.

The USB controller is 99.9% identical to the one in the Coldfire where the same technique is used.

Maybe the USB clock is not configured correctly?

 

There are USB device examples that can be loaded to KWIKSTIK or Tower board at http://www.utasker.com/SW_Demos.html so that you can check your HW.

 

Regards

 

Mark

 

0 件の賞賛
返信