USB_HOST problem in kl26z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB_HOST problem in kl26z

1,545件の閲覧回数
arthshah
Contributor II

hello kerryzhou‌

i am working on USB_Host_MSD in kl26z.

example given in K.S.D.K is working fine but whenever i add some other file releted to other functionality there are problem on USB_HOST.

i just added new file to example project. nothing else.

even not calling extra function from other file.

USB_HOST give me that type of error

"assertion "handler" failed: file "C:/Freescale/KSDK_1.3.0/platform/osa/src/fsl_os_abstraction_bm.c", line 624, function: OSA_TaskDestroy"

why this happen?

please help me to solve this issue with yours ideas.

Thanks,

Arth Shah

ラベル(1)
0 件の賞賛
返信
1 返信

1,473件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Arth,

  I highly suggest you try our newest KSDK2.X for KL26.

  Please download the KSDK2.3_FRDM_KL26Z from this link:

Welcome | MCUXpresso SDK Builder 

  Select the board as FRDM-KL26, then generate the code and download it, you can try to add other file, if you still have problem about it, please let me know.

 SDK1.3 is very old, we won't update that package even it has bugs.


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信