USB Driver under Win7 x64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Driver under Win7 x64

8,841 Views
soil_sci
Contributor I

I have loaded the K60 Tower kit with the USB CDC Device project. When connecting to a Win7 x64 computer and selecting the Freescale_CDC_Driver_Kinetis.inf file, Windows pops up a window that the driver is ont x64 compatible. Is there a Win7 x64 driver for the CDC application?

0 Kudos
Reply
6 Replies

5,552 Views
gustavod
Contributor III

I have attached the correct CDC driver for Windows 32 and 64 bits.

 

Regards.

0 Kudos
Reply

5,552 Views
drone007
Contributor I

Can you please link the 64 bit driver? I have been searching all over for it to test a CDC application with Windows 7.

0 Kudos
Reply

5,552 Views
gustavod
Contributor III

Hi Soil,

 

We made a new .inf file that worked for us. I have attached the file to this message.

Please let me know if it worked.

 

Regards,

Gustavo

0 Kudos
Reply

5,552 Views
soil_sci
Contributor I

I get the same Win7 error message:

I am just trying the provided USB Device project.

I have other projects working on the tower, but this is the only USB app.

0 Kudos
Reply

5,552 Views
admin
Specialist II

Did your device enumerate? The device needs to be enumerated by the PC before you can update the driver software, otherwise you'll get an error message similar to the one you describe.

 

That being said, I wasn't able to get version 3.1 of Freescale's USB stack to enumerate properly. However, I was able to get version 3.0 to work with a custom .inf file under Windows 7 x64. Freescale's USB CDC implementation is standard so you can use the built-in Windows driver and create your own .inf file to load it.

 

This sounds a lot harder than it actually is. Follow the instructions here, and you'll be able to create a custom .inf in under a minute. Here's the default Vendor ID and Product ID line from v3.0 to get you started:

 

%FreescaleCDC%=DriverInstall, USB\VID_2504&PID_0300

 

Good luck!

0 Kudos
Reply

5,552 Views
gustavod
Contributor III

Hi Soil,

 

All i can say is that it is working for us. However, we made our project based on the Freescale USB stack 3.0 You can try our project by downloading the code:

 

This is the project with USB CDC for Codewarrior 10.1:

http://brtos.googlecode.com/files/BRTOS%201.65%20Kinetis%20-%20USB.rar

 

and the same project with SD card and TWR-LCD:

http://brtos.googlecode.com/files/BRTOS%201.66%20Kinetis%20-%20SD%20card%20-%20BMP%2024%20bit.rar

 

Best regards,

Gustavo

 

 

0 Kudos
Reply