USB CDC host receiving unsolicited data from a device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CDC host receiving unsolicited data from a device

4,276件の閲覧回数
tarikaweimrin
Contributor III

I have 2 KL26Z micros talking to each other, one is the host and the other is a CDC device.  I am using the USB stack 4.1.1 I can use the serial_write and serial_read functionality from the host to send and receive data from the device when I know that the device is sending data.  How do I determine if the device has sent unexpected data that needs to be read and the amount of data sent by the device to read?  Is there a flag set somewhere or a callback that I haven't been able to find yet?


Any help would be appreciated.

ラベル(1)
タグ(5)
0 件の賞賛
返信
6 返答(返信)

4,106件の閲覧回数
mjbcswitzerland
Specialist V

Hi

A USB device cannot send data without the host allowing it to, by sending an IN packet which it either responds to or sends a NAK back to.

The host defines the bandwidth available and so will normally be sending IN packets on bulk endpoints whenever there is nothing else to send - the device will therefore be able to return data almost all the time in such an arrangement and the host's DATA reception interrupt will inform of its arrival.

If your host is however not sending IN packets when it is not actually expecting to read data the device will not be able to send anything.

Regards

Mark

0 件の賞賛
返信

4,106件の閲覧回数
tarikaweimrin
Contributor III

Is that in addition to sending the SOF tokens continuously?

0 件の賞賛
返信

4,106件の閲覧回数
mjbcswitzerland
Specialist V

Hi

SOF tokens only define the framework (1ms for FS and 125us for HS) timing but don't allow the device to do anything. [Newer Kinetis parts with crystal-less USB (optionally) use this to re-synchronise the local 48MHz oscillator].

The host must then define the bandwidth allocation (interrupt, isochronous, bulk, depending on the types and number of devices connected) and send IN tokens whenever a device may respond with data.

Regards

Mark

0 件の賞賛
返信

4,106件の閲覧回数
tarikaweimrin
Contributor III

Is there any example code doing this?

0 件の賞賛
返信

4,106件の閲覧回数
mjbcswitzerland
Specialist V

Hi

I think that setting

TOKEN = ((IN_PID << 4) | ENDPOINT_in_question);

will cause the host to poll.

Regards

Mark

0 件の賞賛
返信

4,106件の閲覧回数
tarikaweimrin
Contributor III

Makes sense, I will try that. Thanks

0 件の賞賛
返信