USB CDC K60 virtual com problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB CDC K60 virtual com problem

ソリューションへジャンプ
2,329件の閲覧回数
josei
Contributor II

I´m using USB CDC Vritural Com Example (MQX 4.1)  on a own desing borad K60. The usb enumerate correctly on a desktop PC, send and recibe data. But when I  connect a notebook the device not enumarate.

The usb schematics is:

usbK60-EGSE-CU.PNG

The K60 ucontroller is powered by an external regulator

My software configuration is like:

SO: W7 64bit

RTOS: MQX 4.1.1

HW:MK60DN512ZVLQ10 - 144LQFP

Tool: CW10.6

To discard problems in the notebook drivers made a test with a frdmk64 and is listed correctly.

Someone can help me with this problem?

タグ(3)
1 解決策
2,155件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi Jose,

There is a major problem with your schematic. VOUT33 should be connected with 2.2uF. Otherwise there will not be stable 3.3V output on it. The internal USB transceiver relies on having 3.3V output on VOUT33 to operate correctly. Please try to add the cap.

Hao

元の投稿で解決策を見る

2 返答(返信)
2,156件の閲覧回数
cutworth
NXP Employee
NXP Employee

Hi Jose,

There is a major problem with your schematic. VOUT33 should be connected with 2.2uF. Otherwise there will not be stable 3.3V output on it. The internal USB transceiver relies on having 3.3V output on VOUT33 to operate correctly. Please try to add the cap.

Hao

2,155件の閲覧回数
josei
Contributor II

Thank Hao.

Im put the capacitor and work fine!!

Regards

0 件の賞賛
返信