USB Audio speaker

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Audio speaker

1,692件の閲覧回数
kyleyang
Contributor IV

Hi

I used FRDM-K66F to created a USB audio speaker application based on K21F KSDK 2.0 USB example code.

Basically the function is works in 16bit/16kHz, but when I try to increase the sample rate to 48kHz.

The function is not works.

Is there any one have similar experience before?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,499件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Customer also could refer KSDK software for TWR-K65F180M board [usb dev_audio_speaker] demo.

For the FRDM-K66F use the different codec chip DA7212, customer need to check the DA7212 codec driver related codes. 


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信