[URGRENT] Can't program brand new chip on K22F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[URGRENT] Can't program brand new chip on K22F

跳至解决方案
2,543 次查看
michaelheidinge
Contributor III

Hello,

my setup: Freedom K22F with MBED Firmware

custom board, cleanly soldered. Connections verified.

Problem: I cannot program the K22F MCU. The reset pin is oscillating (very short hight) and the programmer cannot reset the MCU.

Question: How can I program the MCU MK22FN512 now?

Please help quick, I'm in the hurry.

-Michael

0 项奖励
回复
1 解答
2,430 次查看
michaelheidinge
Contributor III

Solved this issue by buying Segger JLink. Sorry to tell, but OpenOCD does not really work with custom boards.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,431 次查看
michaelheidinge
Contributor III

Solved this issue by buying Segger JLink. Sorry to tell, but OpenOCD does not really work with custom boards.

0 项奖励
回复
2,429 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I would recommend customer update the FRDM-K22F OpenSDA V2.1 firmware with Segger J-Link firware (downloaded related J-Link firmware from here).

After the FRDM-K22F OpenSDA firmware updated to J-Link, customer can download [J-Link Software and Documents Pack], using J-Link Commander tool input "unlock Kinetis" command to unlock target MCU.

After that, customer can try using J-Link tool to program the target MCU.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复