UART with KEA8 micro

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART with KEA8 micro

1,389件の閲覧回数
santhoshkumarsi
Contributor I

We want use UART for serial communication with GPS chip on KEA8 micro,Prot pins PTB0 and PTB1 are assigned for UART as ALT4,do we need to make any specific setting to use ALT4 functionality on port pins.

Thanks in Advance.

0 件の賞賛
返信
1 返信

1,292件の閲覧回数
mjbcswitzerland
Specialist V

Hi

KEA8's UART0 is ALT2 on PTB port (not ALT4)

In the uTasker project this is set with:
_CONFIG_PERIPHERAL(B, 0, (PB_0_UART0_RX | UART_PULL_UPS));       // UART0_RX on PB0 (alt. function 2)
_CONFIG_PERIPHERAL(B, 1, (PB_1_UART0_TX | UART_PULL_UPS));       // UART0_TX on PB1 (alt. function 2)


To use the alternative pins on port A instead this would have to be selected with
SIM_PINSEL0 |= (SIM_PINSEL_UART0PS);
and then the pins with

_CONFIG_PERIPHERAL(A, 2, (PA_2_UART0_RX | UART_PULL_UPS));       // UART0_RX on PA2 (alt. function 2)
_CONFIG_PERIPHERAL(A, 3, (PA_3_UART0_TX | UART_PULL_UPS));       // UART0_TX on PA3 (alt. function 2)

Simulation below showing the Rx pin function being checked.

Regards

Mark

pastedImage_4.png

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KEA8:
- http://www.utasker.com/kinetis/TRK-KEA8.html
S32 Design Studio: http://www.utasker.com/kinetis/compilers.html#S32

Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html

0 件の賞賛
返信