UART on KL05Z.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,063件の閲覧回数
nguyennhatminh
Contributor IV

Hi Pro,

I'm trying to use UART to communicate between my computer and KL05Z (Rev B1) by using PE as this tutorial

http://mcuoneclipse.com/2012/10/14/tutorial-printf-and-hello-world-with-the-freedom-kl25z-board/

I have the problem is i don't know which pins UART of KL05Z32M is used to connect to open SDA.

On the schematic http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KL05Z_SCH.pdf?&Parent... shows two pairs UART0 (Pin No 17, 18 ; Pin 23,24 sheet 3 of 5). But in sheet 4 of 5 shows UART1_TX_TGTMCU and UART1_RX_TGTMCU ( on Target MCU KL05Z32M , I think) are connected to OpenSDA.

My question is which pins UART of MCU KL05z32 is connected to OpenSDA ?

Please help me on this issue.

Thank you.

Minh

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,766件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

According to the schematics, in FRDM-KL05Z the OpenSDA interface is connected to the target MCU (KL05Z32) by the pins 17 and 18 (PTB1 and PTB2). This is also mentioned in the FRDM-KL05 User Manual, in two sections:

UART_SDA.png

Hope this helps!


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,767件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

According to the schematics, in FRDM-KL05Z the OpenSDA interface is connected to the target MCU (KL05Z32) by the pins 17 and 18 (PTB1 and PTB2). This is also mentioned in the FRDM-KL05 User Manual, in two sections:

UART_SDA.png

Hope this helps!


Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信