UART in VLPR\VLPS[MKW24D512]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART in VLPR\VLPS[MKW24D512]

1,397 Views
yuhuixuan
Contributor I

I want to use the uart communicate in a low power. In VLPR the UART moudle is active and the current is 2mA. In VLPS the UART is not work.

So Is there any other way that the UART can work and the power cost is low?

And in the VLPS mode the UART can work. Is the current is 2mA in the VLPS mode? If there is less than 2mA. Please send it to me the demo.

And in the VLPS mode. Use the fast IRC 4m no divide. I confige the baud. But the UART doesn't receive the right byte. Why this happen?

Labels (1)
0 Kudos
Reply
1 Reply

1,189 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Yu Huixuan

As you can see in module operation in low power modes, UART module is just enable in VLPR and VLPW modes, so in VLPS mode, uart module register states and associated memories are retained but it is not working:

pastedImage_8.png

So in VLPS mode it doesn't matter that you configure your baudrate it will not work until you set your device in VLPR or RUN mode.


Hope this information helps you
Have a great day,
Jorge Alcala

0 Kudos
Reply