UART FIFO SIZE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART FIFO SIZE

跳至解决方案
3,019 次查看
peterruesch
Contributor IV

Hi,

using EmbSysRegView in Processor Expert, I suspect the UART{0,1} RX/TX FIFO size on my part (MK65) is 8 Byte. The other UARTS don't have a FIFO.

in what documents from Freescale can I find such information?

The Datasheet is not giving a single search hit for "fifo"...

and the reference manual states " See the Chip Configuration details for more information on the FIFO size supported for each UART instance"...

Where is this frequently referenced "Chip Configuration details" Document???

1 解答
2,603 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Peter:

The FIFO sizes are defined at the beginning of the UART chapter in the Reference Manual, in points 5 and 6, see below:

K65_UART_FIFOs.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,604 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Peter:

The FIFO sizes are defined at the beginning of the UART chapter in the Reference Manual, in points 5 and 6, see below:

K65_UART_FIFOs.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------