Two I2C interfaces AND MDIO / MDC possible?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two I2C interfaces AND MDIO / MDC possible?

3,454 Views
pk2
Contributor III

I am working on a design that requires an RMII Ethernet interface and two I2C interfaces (one master and 1 slave).  Will the MK60FN1M0VLQ12 support this?  WIll the MDIO / MDC interface (pins 81 and 82 for this device) and both I2C0 and I2C1 work at the same time (i.e. simultaneously)?

Labels (1)
0 Kudos
Reply
3 Replies

2,496 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, PK2

No, you can use I2C and RMII at the same time. I suggest you use Pin 137,138 for I2C0.

Hope my reply can help you.

Best Regards

Paul

2,496 Views
pk2
Contributor III

Is there a reason I can not use pins 83 and 84?

0 Kudos
Reply

2,496 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, PK2

Yes, you can use pin 83 and 84.